Data structure of the connection_iq_report event.

Public Attributes#

uint16_t
uint8_t
uint8_t
uint8_t
int8_t
uint8_t

Public Attribute Documentation#

status#

uint16_t sl_bt_evt_cte_receiver_connection_iq_report_s::status

Status of CTE IQ sampling


connection#

uint8_t sl_bt_evt_cte_receiver_connection_iq_report_s::connection

Connection handle or periodic advertising synchronization handle


phy#

uint8_t sl_bt_evt_cte_receiver_connection_iq_report_s::phy

The PHY on which the packet is received.

  • 1: 1M PHY

  • 2: 2M PHY


channel#

uint8_t sl_bt_evt_cte_receiver_connection_iq_report_s::channel

The channel on which the CTE packet was received


rssi#

int8_t sl_bt_evt_cte_receiver_connection_iq_report_s::rssi

RSSI in the received CTE packet. Unit: dBm


rssi_antenna_id#

uint8_t sl_bt_evt_cte_receiver_connection_iq_report_s::rssi_antenna_id

The ID of the antenna on which RSSI was measured


cte_type#

uint8_t sl_bt_evt_cte_receiver_connection_iq_report_s::cte_type

The CTE type

  • 0: AoA CTE response

  • 1: AoD CTE response with 1us slots

  • 2: AoD CTE response with 2us slots


slot_durations#

uint8_t sl_bt_evt_cte_receiver_connection_iq_report_s::slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each


event_counter#

uint16_t sl_bt_evt_cte_receiver_connection_iq_report_s::event_counter

The event counter of the connection


samples#

uint8array sl_bt_evt_cte_receiver_connection_iq_report_s::samples

IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...)