sl_bt_evt_dfu_boot_failure#

This event indicates that an error, which prevents the device from booting, has occurred in bootloader.

Modules#

sl_bt_evt_dfu_boot_failure_s

Macros#

#define
sl_bt_evt_dfu_boot_failure_id 0x010000a0

Identifier of the boot_failure event.

Typedef Documentation#

sl_bt_evt_dfu_boot_failure_t#

typedef struct sl_bt_evt_dfu_boot_failure_s sl_bt_evt_dfu_boot_failure_t

Definition at line 176 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h