sl_bt_evt_external_bondingdb_data_ready#

Indicates that stack has received all the necessary bonding data from the application and is now fully functional.

Modules#

sl_bt_evt_external_bondingdb_data_ready_s

Macros#

#define

Identifier of the data_ready event.

Typedef Documentation#

sl_bt_evt_external_bondingdb_data_ready_t#

typedef struct sl_bt_evt_external_bondingdb_data_ready_s sl_bt_evt_external_bondingdb_data_ready_t

Definition at line 10897 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_external_bondingdb_data_ready_id#

#define sl_bt_evt_external_bondingdb_data_ready_id
Value:
0x025c00a0

Identifier of the data_ready event.


Definition at line 10887 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h