sl_bt_evt_gatt_mtu_exchanged#
Indicates that an ATT_MTU exchange procedure is completed.
The mtu
parameter describes new MTU size. MTU size 23 is used before this event is received.
Modules#
sl_bt_evt_gatt_mtu_exchanged_s
Macros#
#define
Identifier of the mtu_exchanged event.
Typedef Documentation#
sl_bt_evt_gatt_mtu_exchanged_t#
typedef struct sl_bt_evt_gatt_mtu_exchanged_s sl_bt_evt_gatt_mtu_exchanged_t
Definition at line 7115
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_gatt_mtu_exchanged_id#
#define sl_bt_evt_gatt_mtu_exchanged_id
Value:0x000900a0
Identifier of the mtu_exchanged event.
Definition at line 7104
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h