Data structure of the attribute_value event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_server_attribute_value_s::connection
Connection handle
Definition at line
8682
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
attribute#
uint16_t sl_bt_evt_gatt_server_attribute_value_s::attribute
Attribute Handle
Definition at line
8683
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
att_opcode#
uint8_t sl_bt_evt_gatt_server_attribute_value_s::att_opcode
Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.
Definition at line
8684
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
offset#
uint16_t sl_bt_evt_gatt_server_attribute_value_s::offset
Value offset
Definition at line
8687
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
value#
uint8array sl_bt_evt_gatt_server_attribute_value_s::value
Value
Definition at line
8688
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h