Data structure of the characteristic_status event.

Public Attributes#

uint8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_server_characteristic_status_s::connection

Connection handle


Definition at line 8800 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

characteristic#

uint16_t sl_bt_evt_gatt_server_characteristic_status_s::characteristic

GATT characteristic handle. This value is normally received from the gatt_characteristic event.


Definition at line 8801 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

status_flags#

uint8_t sl_bt_evt_gatt_server_characteristic_status_s::status_flags

Enum sl_bt_gatt_server_characteristic_status_flag_t. Describes whether Client Characteristic Configuration was changed or if a confirmation was received. Values:

  • sl_bt_gatt_server_client_config (0x1): Characteristic client configuration has been changed.

  • sl_bt_gatt_server_confirmation (0x2): Characteristic confirmation has been received.


Definition at line 8804 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

client_config_flags#

uint16_t sl_bt_evt_gatt_server_characteristic_status_s::client_config_flags

Enum sl_bt_gatt_server_client_configuration_t. This field carries the new value of the Client Characteristic Configuration. If the status_flags is 0x2 (confirmation received), the value of this field can be ignored.


Definition at line 8815 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

client_config#

uint16_t sl_bt_evt_gatt_server_characteristic_status_s::client_config

The handle of client-config descriptor.


Definition at line 8822 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h