You are viewing documentation for version:
sl_bt_evt_pawr_sync_opened#
Indicates that synchronization to a Periodic Advertising with Responses (PAwR) train has been opened by scanning.
See command sl_bt_sync_scanner_open.
Modules#
sl_bt_evt_pawr_sync_opened_s
Macros#
#define
Identifier of the opened event.
Typedef Documentation#
sl_bt_evt_pawr_sync_opened_t#
typedef struct sl_bt_evt_pawr_sync_opened_s sl_bt_evt_pawr_sync_opened_t
Definition at line 4806
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_pawr_sync_opened_id#
#define sl_bt_evt_pawr_sync_opened_id
Value:0x005400a0
Identifier of the opened event.
Definition at line 4725
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h