sl_bt_evt_periodic_sync_transfer_received#
Indicates that synchronization information for a periodic advertising train that does not have subevents or response slots has been received.
See PAST Receiver.
Modules#
sl_bt_evt_periodic_sync_transfer_received_s
Typedefs#
Macros#
#define
sl_bt_evt_periodic_sync_transfer_received_id 0x015300a0
Identifier of the transfer_received event.
Typedef Documentation#
sl_bt_evt_periodic_sync_transfer_received_t#
typedef struct sl_bt_evt_periodic_sync_transfer_received_s sl_bt_evt_periodic_sync_transfer_received_t
Definition at line
4637
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_periodic_sync_transfer_received_id#
#define sl_bt_evt_periodic_sync_transfer_received_idValue:
0x015300a0
Identifier of the transfer_received event.
Definition at line
4571
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h