Data structure of the error event.

Public Attributes#

uint16_t

Public Attribute Documentation#

reason#

uint16_t sl_bt_evt_system_error_s::reason

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 822 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

data#

uint8array sl_bt_evt_system_error_s::data

Data related to the error; this field can be empty.


Definition at line 823 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h