Periodic Advertising Configuration Flags#

Defines configuration flags for periodic advertising.

Macro Definition Documentation#

SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER#

#define SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER
Value:
0x1

Include the TX power in advertising packets.


Definition at line 2956 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING#

#define SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING
Value:
0x2

Automatically start the extended advertising on the advertising set. The advertising will be started in non-connectable and non-scannable mode.


Definition at line 2960 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h