Filter Accept List#
Filter Accept List.
Provides support for adding and removing devices from the Filter Accept List in the Bluetooth controller.
The Filter Accept List allows filtering transmissions from other Bluetooth devices so that the local device only receives/accepts transmissions from the devices that it's interested in or wants to communicate with. Operations that support filtering provide a means to control how the Filter Accept List is used:
- For advertising, use the command sl_bt_advertiser_configure and - flagsbits SL_BT_ADVERTISER_USE_FILTER_FOR_SCAN_REQUESTS and SL_BT_ADVERTISER_USE_FILTER_FOR_CONNECTION_REQUESTS to control the advertising filter policy
- For scanning, use the command sl_bt_scanner_set_parameters_and_filter to control the scanning filter policy 
Functions#
Macros#
Function Documentation#
sl_bt_accept_list_add_device_by_bonding#
sl_status_t sl_bt_accept_list_add_device_by_bonding (uint32_t bonding)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | bonding | The bonding handle | 
Add a device to the Filter Accept List based on its bonding handle.
This command returns the error SL_STATUS_BT_CTRL_CONTROLLER_BUSY if the Filter Accept List is currently used by scanning filter policy, advertising filter policy, or by initiator filter policy, i.e. initiating connection to devices on the Filter Accept List. If the list is currently in use, the application needs to first stop the operation that uses the Filter Accept List, then add a device to the Filter Accept List, and then restart the operation that uses the Filter Accept List.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_accept_list_add_device_by_address#
sl_status_t sl_bt_accept_list_add_device_by_address (bd_addr address, uint8_t address_type)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| bd_addr | [in] | address | Bluetooth address of the peer device | 
| uint8_t | [in] | address_type | Enum sl_bt_gap_address_type_t. The peer device address type. Values: 
 | 
Add a device to the Filter Accept List based on its identity address.
Use the special address type sl_bt_gap_anonymous_address to add an entry that matches all advertisements sent with no address.
This command returns the error SL_STATUS_BT_CTRL_CONTROLLER_BUSY if the Filter Accept List is currently used by scanning filter policy, advertising filter policy, or by initiator filter policy, i.e. initiating connection to devices on the Filter Accept List. If the list is currently in use, the application needs to first stop the operation that uses the Filter Accept List, then add a device to the Filter Accept List, and then restart the operation that uses the Filter Accept List.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_accept_list_remove_device_by_bonding#
sl_status_t sl_bt_accept_list_remove_device_by_bonding (uint32_t bonding)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | bonding | The bonding handle | 
Remove a device from the Filter Accept List based on its bonding handle.
This command returns the error SL_STATUS_BT_CTRL_CONTROLLER_BUSY if the Filter Accept List is currently used by scanning filter policy, advertising filter policy, or by initiator filter policy, i.e. initiating connection to devices on the Filter Accept List. If the list is currently in use, the application needs to first stop the operation that uses the Filter Accept List, then remove a device from the Filter Accept List, and then restart the operation that uses the Filter Accept List.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_accept_list_remove_device_by_address#
sl_status_t sl_bt_accept_list_remove_device_by_address (bd_addr address, uint8_t address_type)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| bd_addr | [in] | address | Bluetooth address of the peer device | 
| uint8_t | [in] | address_type | Enum sl_bt_gap_address_type_t. The peer device address type. Values: 
 | 
Remove a device from the Filter Accept List based on its identity address.
Use the special address type sl_bt_gap_anonymous_address to remove an entry that matches all advertisements sent with no address.
This command returns the error SL_STATUS_BT_CTRL_CONTROLLER_BUSY if the Filter Accept List is currently used by scanning filter policy, advertising filter policy, or by initiator filter policy, i.e. initiating connection to devices on the Filter Accept List. If the list is currently in use, the application needs to first stop the operation that uses the Filter Accept List, then remove a device from the Filter Accept List, and then restart the operation that uses the Filter Accept List.
Returns
- SL_STATUS_OK if successful. Error code otherwise. 
sl_bt_accept_list_remove_all_devices#
sl_status_t sl_bt_accept_list_remove_all_devices ()
Remove all devices from the Filter Accept List.
This command returns the error SL_STATUS_BT_CTRL_CONTROLLER_BUSY if the Filter Accept List is currently used by scanning filter policy, advertising filter policy, or by initiator filter policy, i.e. initiating connection to devices on the Filter Accept List. If the list is currently in use, the application needs to first stop the operation that uses the Filter Accept List, and then remove all devices from the Filter Accept List.
Returns
- SL_STATUS_OK if successful. Error code otherwise.