NCP Host Communication Interface#
Component that provides the Bluetooth Network Co-Processor (NCP) host communication interface. This is a No-Code component.
Functions#
void
sl_ncp_host_com_init(void)
void
sl_ncp_host_com_write(uint32_t len, uint8_t *data)
int32_t
sl_ncp_host_com_read(uint32_t len, uint8_t *data)
int32_t
sl_ncp_host_com_peek(void)
bool
Macros#
#define
SL_NCP_HOST_COM_BUF_SIZE (260)
Function Documentation#
sl_ncp_host_com_init#
void sl_ncp_host_com_init (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
NCP host communication initialization.
sl_ncp_host_com_write#
void sl_ncp_host_com_write (uint32_t len, uint8_t * data)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | len | |
| uint8_t * | N/A | data |
Transmit function
sl_ncp_host_com_read#
int32_t sl_ncp_host_com_read (uint32_t len, uint8_t * data)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | len | |
| uint8_t * | N/A | data |
Receive function
sl_ncp_host_com_peek#
int32_t sl_ncp_host_com_peek (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Gives back already received message length.
sl_ncp_host_is_ok_to_sleep#
bool sl_ncp_host_is_ok_to_sleep (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |