sl_bt_evt_connection_set_parameters_failed#

Triggered when the peer device rejected an L2CAP connection parameter update request as a result of calling command sl_bt_connection_set_parameters to change connection parameters on the sl_bt_connection_role_peripheral role.

Modules#

sl_bt_evt_connection_set_parameters_failed_s

Macros#

#define

Identifier of the set_parameters_failed event.

Typedef Documentation#

sl_bt_evt_connection_set_parameters_failed_t#

typedef struct sl_bt_evt_connection_set_parameters_failed_s sl_bt_evt_connection_set_parameters_failed_t

Macro Definition Documentation#

sl_bt_evt_connection_set_parameters_failed_id#

#define sl_bt_evt_connection_set_parameters_failed_id
Value:
0x100600a0

Identifier of the set_parameters_failed event.