sl_bt_evt_cs_test_end_completed#

This event is generated when the local controller stops the ongoing CS test as the result of calling the sl_bt_cs_test_end command.

Modules#

sl_bt_evt_cs_test_end_completed_s

Macros#

#define

Identifier of the end_completed event.

Typedef Documentation#

sl_bt_evt_cs_test_end_completed_t#

typedef struct sl_bt_evt_cs_test_end_completed_s sl_bt_evt_cs_test_end_completed_t

Definition at line 13772 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_cs_test_end_completed_id#

#define sl_bt_evt_cs_test_end_completed_id
Value:
0x005a00a0

Identifier of the end_completed event.


Definition at line 13762 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h