sl_bt_evt_gatt_server_attribute_value#

Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.

The parameter att_opcode describes which GATT procedure was used to change the value.

Modules#

sl_bt_evt_gatt_server_attribute_value_s

Macros#

#define

Identifier of the attribute_value event.

Typedef Documentation#

sl_bt_evt_gatt_server_attribute_value_t#

typedef struct sl_bt_evt_gatt_server_attribute_value_s sl_bt_evt_gatt_server_attribute_value_t

Definition at line 9323 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_gatt_server_attribute_value_id#

#define sl_bt_evt_gatt_server_attribute_value_id
Value:
0x000a00a0

Identifier of the attribute_value event.


Definition at line 9307 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h