Data structure of the opened event.
Public Attribute Documentation#
address_type#
uint8_t sl_bt_evt_pawr_sync_opened_s::address_type
Enum sl_bt_gap_address_type_t.
Advertiser address type.
If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:
0: Public address
1: Random address
If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:
sl_bt_gap_public_address (0x0): Public device address
sl_bt_gap_static_address (0x1): Static device address
sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address
sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address
sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)
sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)
adv_phy#
uint8_t sl_bt_evt_pawr_sync_opened_s::adv_phy
Enum sl_bt_gap_phy_t. The advertiser PHY. Values:
sl_bt_gap_phy_1m (0x1): 1M PHY
sl_bt_gap_phy_2m (0x2): 2M PHY
sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)
adv_interval#
uint16_t sl_bt_evt_pawr_sync_opened_s::adv_interval
The periodic advertising interval. Value in units of 1.25 ms
Range: 0x06 to 0xFFFF
Time range: 7.5 ms to 81.92 s
clock_accuracy#
uint16_t sl_bt_evt_pawr_sync_opened_s::clock_accuracy
Enum sl_bt_sync_advertiser_clock_accuracy_t. The advertiser clock accuracy.
num_subevents#
uint8_t sl_bt_evt_pawr_sync_opened_s::num_subevents
The number of subevents.
Range: 0x01 to 0x80
subevent_interval#
uint8_t sl_bt_evt_pawr_sync_opened_s::subevent_interval
Subevent interval. Value in units of 1.25 ms.
Range: 0x06 to 0xFF
Time range: 7.5 ms to 318.75 ms
response_slot_delay#
uint8_t sl_bt_evt_pawr_sync_opened_s::response_slot_delay
Time between the advertising packet in a subevent and the first response slot. Value in units of 1.25 ms.
Range: 0x01 to 0xFE
Time range: 1.25 ms to 317.5 ms
response_slot_spacing#
uint8_t sl_bt_evt_pawr_sync_opened_s::response_slot_spacing
Time between the start of response slots in a subevent. Value in units of 0.125 ms.
Range: 0x02 to 0xFF
Time range: 0.25 ms to 31.875 ms
bonding#
uint8_t sl_bt_evt_pawr_sync_opened_s::bonding
Bonding handle. Values:
SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding
Other: Bonding handle