sl_bt_evt_sync_closed#

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

The synchronization establishment procedure can be canceled explicitly by the application by issuing command sl_bt_sync_close, or internally due to synchronization failing. Synchronization can fail for example due to incompatible sync CTE type.

Modules#

sl_bt_evt_sync_closed_s

Macros#

#define

Identifier of the closed event.

Typedef Documentation#

sl_bt_evt_sync_closed_t#

typedef struct sl_bt_evt_sync_closed_s sl_bt_evt_sync_closed_t

Definition at line 4241 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_sync_closed_id#

#define sl_bt_evt_sync_closed_id
Value:
0x014200a0

Identifier of the closed event.


Definition at line 4230 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h