CS Initiator Display#
Prints Channel Sounding (CS) Initiator status information to the LCD of the WSTK.
Modules#
cs_initiator_display_content_t
cs_initiator_display_instance_t
Enumerations#
Display rows.
UI alignment.
Functions#
Macros#
Enumeration Documentation#
cs_initiator_display_status_t#
cs_initiator_display_status_t
| Enumerator | |
|---|---|
| CS_INITIATOR_DISPLAY_STATUS_CONNECTED | |
| CS_INITIATOR_DISPLAY_STATUS_SCANNING | |
| CS_INITIATOR_DISPLAY_STATUS_ESTIMATE | |
| CS_INITIATOR_DISPLAY_STATUS_INITIALIZED | |
| CS_INITIATOR_DISPLAY_STATUS_UNINITIALIZED | |
| CS_INITIATOR_DISPLAY_STATUS_SPOOFED | |
cs_initiator_display_row_t#
cs_initiator_display_row_t
Display rows.
| Enumerator | |
|---|---|
| ROW_MODE | |
| ROW_INSTANCE_NUM | |
| ROW_STATUS_TEXT | |
| ROW_STATUS_VALUE | |
| ROW_DISTANCE_TEXT | |
| ROW_DISTANCE_VALUE | |
| ROW_RAW_DISTANCE_TEXT | |
| ROW_RAW_DISTANCE_VALUE | |
| ROW_LIKELINESS_TEXT | |
| ROW_LIKELINESS_VALUE | |
| ROW_RSSI_DISTANCE_TEXT | |
| ROW_RSSI_DISTANCE_VALUE | |
| ROW_BIT_ERROR_RATE_TEXT | |
| ROW_BIT_ERROR_RATE_VALUE | |
cs_initiator_display_alignment_t#
cs_initiator_display_alignment_t
UI alignment.
| Enumerator | |
|---|---|
| CS_INITIATOR_DISPLAY_ALIGNMENT_LEFT | |
| CS_INITIATOR_DISPLAY_ALIGNMENT_CENTER | |
| CS_INITIATOR_DISPLAY_ALIGNMENT_RIGHT | |
Function Documentation#
cs_initiator_display_create_instance#
sl_status_t cs_initiator_display_create_instance (uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | conn_handle | Connection handle |
Create new display instance Returns
SL_STATUS_OK on success
cs_initiator_display_delete_instance#
sl_status_t cs_initiator_display_delete_instance (uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | conn_handle | Connection handle |
Delete display instance The deleted instance will start scanning Returns
SL_STATUS_OK on success
cs_initiator_display_set_measurement_mode#
void cs_initiator_display_set_measurement_mode (sl_bt_cs_mode_t mode, uint8_t algo_mode)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_cs_mode_t | [in] | mode | CS Measurement mode |
| uint8_t | [in] | algo_mode | Algorithm mode |
Set the measurement mode and object tracking mode to display.
cs_initiator_display_insert_new_float_value#
void cs_initiator_display_insert_new_float_value (float new_value, uint8_t row, uint8_t conn_handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [in] | new_value | New value to display |
| uint8_t | [in] | row | Row number to display the value on |
| uint8_t | [in] | conn_handle | Connection handle |
Insert new floating point value to the specified row on the display
cs_initiator_display_insert_new_distance_value#
void cs_initiator_display_insert_new_distance_value (float new_value, uint8_t conn_handle, float percentage, sl_rtl_cs_algo_mode algo_mode)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [in] | new_value | New distance value to display |
| uint8_t | [in] | conn_handle | Connection handle |
| float | [in] | percentage | Percentage of the distance |
| sl_rtl_cs_algo_mode | [in] | algo_mode | Algorithm mode |
Insert new distance value to the display Returns
SL_STATUS_OK on success
cs_initiator_display_insert_new_status#
sl_status_t cs_initiator_display_insert_new_status (uint8_t new_status, uint8_t instance_num)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | new_status | New status to display |
| uint8_t | [in] | instance_num | Instance number to display the status on |
Insert new status to the display Returns
SL_STATUS_OK on success
cs_initiator_display_start_scanning#
void cs_initiator_display_start_scanning (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Start scanning and show it on the display.
cs_initiator_display_update_data#
void cs_initiator_display_update_data (uint8_t instance_num, uint8_t conn_handle, uint8_t status, float distance, float rssi_distance, float likeliness, float bit_error_rate, float raw_distance, float progress_percentage, uint8_t algo_mode, sl_bt_cs_mode_t cs_mode)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | instance_num | Instance number to update |
| uint8_t | [in] | conn_handle | Connection handle |
| uint8_t | [in] | status | Status of the display instance |
| float | [in] | distance | Distance value of the display instance |
| float | [in] | rssi_distance | RSSI distance value of the display instance |
| float | [in] | likeliness | Likeliness value of the display instance |
| float | [in] | bit_error_rate | Bit error rate value of the display instance |
| float | [in] | raw_distance | Raw distance value of the display instance |
| float | [in] | progress_percentage | Progress percentage of the display instance |
| uint8_t | [in] | algo_mode | Algorithm mode of the display instance |
| sl_bt_cs_mode_t | [in] | cs_mode | CS mode of the display instance |
Update the data for a specified display instance
cs_initiator_display_update_instance#
void cs_initiator_display_update_instance (uint8_t instance_num)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | instance_num | Instance number to update |
Update instance values on the display.
cs_initiator_display_on_event#
void cs_initiator_display_on_event (sl_bt_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack. |
Bluetooth stack event handler.
cs_initiator_display_init#
sl_status_t cs_initiator_display_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize the display.
cs_initiator_display_set_alignment#
void cs_initiator_display_set_alignment (cs_initiator_display_alignment_t align)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| cs_initiator_display_alignment_t | [in] | align | text alignment to use |
Set the display text alignment.
cs_initiator_display_write_text_to_instance#
void cs_initiator_display_write_text_to_instance (char * str, uint8_t row, uint8_t instance)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| char * | [in] | str | pointer to the text to print |
| uint8_t | [in] | row | row to print the text on |
| uint8_t | [in] | instance | instance number |
Write text on the LCD.
cs_initiator_display_write_float_to_instance#
void cs_initiator_display_write_float_to_instance (float value, uint8_t row, uint8_t instance)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [in] | value | float value to print |
| uint8_t | [in] | row | row to print the value on |
| uint8_t | [in] | instance | instance number |
Write float value on the LCD.
cs_initiator_display_clear_instance#
void cs_initiator_display_clear_instance (uint8_t instance)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | instance | instance number |
Clear instance values on the display.
cs_initiator_display_clear_row#
void cs_initiator_display_clear_row (uint8_t row)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | row | row to clear |
Clear a specified row on the display.
cs_initiator_display_update#
void cs_initiator_display_update (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Update the display.