ESL Tag core#
Implements the ESL Tag role of the Bluetooth Electronic Shelf Label Profile. It contains the mandatory ESL Tag characteristics, only. Optional features has to be added to the project as separate components, if needed. This component implements all the core functionalities, while also declares the interface of the optional features (and provides the WEAK implementations for them). This is a No-Code component, any additional feature can be added as a component.
Modules#
Typedefs#
ESL Display Info Display Type.
ESL Display Info first class abstract data pointer type.
ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.
ESL LED type.
ESL LED color gamut control type.
ESL LED repeats type.
Functions#
Macros#
Definition for unknown battery voltage level (an implausible value)
Custom psa_key_id_t for ESL AP Sync Key permanent storage (for AES key only)
Custom psa_key_id_t for ESL Response Key permanent storage.
ESL Display Type Assigned Numbers.
3 gray scale displays
4 gray scale displays
8 gray scale displays
16 gray scale displays
Red, black, white displays.
Yellow, black, white displays.
Red, yellow, black, white displays.
7 color displays
16 color displays
Full RGB color space displays.
Unspecified Error: any error condition that is not covered by a specific error code below
Invalid Opcode: The opcode was not recognized.
Invalid State: The request was not valid for the present ESL state.
Invalid Image Index: The Image_Index value was out of range.
Image Not Available: The requested image contained no image data.
Invalid Parameter(s): The parameter value(s) or length did not match the opcode
Capacity Limit: The required response could not be sent as it would exceed the payload size limit
Insufficient Battery: The request could not be processed because of a lack of battery charge
Insufficient Resources: The request could not be processed because of a lack of resources. This may be a temporary condition.
Retry: The ESL is temporarily not able to give a full response (e.g., because the required sensor hardware was asleep) and the AP is asked to try the same command again.
Queue Full: The ESL is temporarily unable to add a further timed command to the queue of pending commands Âthe queue has reached its limit.
Implausible time: The Absolute Time parameter value in the command would result in a delay longer than 48 days (that is, it's a possible overflow)
No Error: 0xFF is reserved for 'no error' indication. For internal use only, and it is Silicon Labs specific.
No report: 0xFE is reserved for 'no error report needed for timed commands' indication. For internal use only, and it is Silicon Labs specific.
Wrapper around esl_core_set_last_error() to clear the last error
Wrapper around esl_core_get_last_error() to check if there's no error
ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.
ESL LED type definition: sRGB.
ESL LED type definition: Monochrome.
ESL LED color gamut / brightness values.
ESL LED color gamut / brightness step percentage.
Function like macro getter for 2-bit brightness value from a gamut value Returns
esl_led_gamut_control_t brightness
Function like macro getter for 2-bit red value from a gamut value Returns
esl_led_gamut_control_t red value
Function like macro getter for 2-bit green value from a gamut value Returns
esl_led_gamut_control_t green value
Function like macro getter for 2-bit blue value from a gamut value Returns
esl_led_gamut_control_t blue value
The command could not be processed successfully.
Acknowledgment of a request to control an LED.
General acknowledgment containing ESL status data.
Acknowledgment of a request to display an image.
Sensor report.
Response data as specified by the vendor of the ESL.
Mask for getting the Tag value from an ESL TLV.
Mask for getting the Length value from an ESL TLV.
Function like macro getter for 'Tag' field from an ESL TLV Returns
tlv_tag_t 'Tag' value of the TLV
Function like macro getter for real 'Length' value from an ESL TLV Returns
tlv_length_t 'Length' value of the TLV
Function like macro for setting the 'Tag' value of a TLV
Function like macro for setting the 'Length' value of a TLV
ESL Display extra parameters count for init_func esl_va_method function.
ESL Display extra parameters count for write_func esl_va_method function.
Typedef Documentation#
esl_display_info_p#
typedef struct esl_display_info_t* esl_display_info_p
ESL Display Info first class abstract data pointer type.
esl_image_object_id_t#
typedef uint8_t esl_image_object_id_t[6] [6]
ESL Service Specification d09r18, Section 3.7.2.4: 48 bit Image Object ID.
Function Documentation#
esl_sensor_battery_init#
sl_status_t esl_sensor_battery_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
esl_sensor_battery_read#
sl_status_t esl_sensor_battery_read (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
esl_sensor_get_battery_voltage_mv#
uint32_t esl_sensor_get_battery_voltage_mv (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
esl_sensor_core_check_battery_level#
void esl_sensor_core_check_battery_level (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
esl_core_encrypt_message#
void * esl_core_encrypt_message (void * msg, uint8_t * len)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | msg | Pointer to the message to be encrypted |
| uint8_t * | N/A | len | len Pointer to a variable containing the length of the message to be encrypted [in bytes] |
Message encryption function Returns
void* Pointer to the encrypted message on success, NULL otherwise.
Note
Also changes the value of *len to the resulting length on successful operation.
esl_core_decrypt_message#
void * esl_core_decrypt_message (void * msg, uint8_t * len)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | msg | Pointer to the message to be decrypted |
| uint8_t * | N/A | len | len Pointer to a variable containing the length of the message to be decrypted [in bytes] |
Message decryption function Returns
void* Pointer to the decrypted message on success, NULL otherwise.
Note
Also changes the value of *len to the resulting length on successful operation.
esl_display_init#
void esl_display_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ESL Tag display component init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.
esl_display_refresh#
sl_status_t esl_display_refresh (uint8_t display_index, uint8_t * image_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | display_index | Selects the display to show the image on. |
| uint8_t * | [out] | image_index | Returns last image set on the refreshed display. |
Refresh the content of the ESL Tag Display. Re-displays the image which was previously set on the given screen. Returns
sl_status_t
esl_display_update#
sl_status_t esl_display_update (uint8_t display_index, uint8_t image_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | display_index | Selects the display to show the image on. |
| uint8_t | [in] | image_index | Selects the image to be shown on the display. |
Update image data on ESL Tag Display. Returns
sl_status_t
esl_display_get_count#
uint8_t esl_display_get_count ()
ESL Display: display count getter Returns
Number of available displays
esl_core_get_last_error#
esl_error_t esl_core_get_last_error (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Gets the last error code Returns
esl_error_t_t
esl_core_set_last_error#
void esl_core_set_last_error (esl_error_t error_code)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| esl_error_t | [in] | error_code | error code |
Sets the last error code
esl_image_init#
void esl_image_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ESL Tag image init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.
esl_image_characteristic_update#
void esl_image_characteristic_update (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ESL Tag image characteristic update. ESL Core component will call this automatically on the bluetooth stack boot event. The real implementation in the ESL Tag Image component will get the display info and write it to the ESL Image Information Characteristic value for the lifecycle of the tag.
esl_image_get_data#
sl_status_t esl_image_get_data (uint8_t image_index, uint16_t * offset, uint16_t buf_size, uint8_t * target_buf)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | image_index | image_index Index of the image to get raw data chunk of |
| uint16_t * | [out] | offset | *offset Size of data already read out |
| uint16_t | [in] | buf_size | buf_size Actual size of the target buffer |
| uint8_t * | [out] | target_buf | *target_buf Buffer address to copy the image chunk into |
Getter for an ESL Tag image raw data chunk
Note
To get full image data this function needs to be called repeatedly until the offset value increases - offset in caller has to be persistent during the process, and usually its value must be set to 0, initially
Returns
sl_status_t
esl_image_get_count#
uint8_t esl_image_get_count (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ESL Tag maximum image count getter Returns
Number of available images
Note
: To be implemented with each custom image storage implementation!
esl_image_reset_storage#
void esl_image_reset_storage (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Reset image storage objects Note
: To be implemented with each custom image storage implementation!
esl_image_unpack_init#
void esl_image_unpack_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Reinit image compression algorithm if it is used
esl_image_unpack_chunk#
sl_status_t esl_image_unpack_chunk (const void * code, const size_t chunk_size, void * data, size_t data_offset, size_t data_length, size_t * decompressed_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const void * | N/A | code | Pointer to the current incoming data chunk |
| const size_t | N/A | chunk_size | Size of the incoming data in bytes |
| void * | N/A | data | Pointer to the target area of unpacking |
| size_t | N/A | data_offset | Current write offset from the start of the unpacking area |
| size_t | N/A | data_length | Maximum size of the unpacking area |
| size_t * | N/A | decompressed_length | Size of the last chunk written to target area |
Unpack single chunk of received image data if compression is used
Returns
Returns SL_STATUS_OK on success, SL_STATUS_FAIL if decompression fails or SL_STATUS_WOULD_OVERFLOW if an uncompressed data chunk is too big to write to the target area.
Unpacks data slices if the otf_decompressor component is used or copy uncompressed data to the target area, otherwise.
esl_led_init#
void esl_led_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ESL Tag LED init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.
esl_led_control#
sl_status_t esl_led_control (esl_led_control_t * control_param)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| esl_led_control_t * | [in] | control_param | ESL LED control parameters defined by the ESL standard - excluding the ESL ID. |
ESL Tag LED control function Note
updates the active LED bit in ESL basic state register according to the actual status of all LEDs
Returns
sl_status_t
esl_led_is_srgb#
bool esl_led_is_srgb (uint8_t led_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | led_index |
Get ESL Tag LED count Returns
Number of available LEDs
esl_core_respones_init#
void esl_core_respones_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Init ESL Tag responses queue. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.
esl_core_build_response#
sl_status_t esl_core_build_response (tlv_t tlv, const void * input_data)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| tlv_t | [in] | tlv | The TLV to create the response stream for |
| const void * | [in] | input_data | can be a pointer to the basic status, led status etc. |
Create response byte stream for single TLV based on input data and error status (if any) then puts the response stream into a circular buffer. The resulting output length of a single TLV will be the length encoded in that particular TLV + 1 byte as per ESL specification. Multiple response streams will be then concatenated on consecutive calls up to the maximum length limit of 48 bytes for multiple response data. Note
the actual length of the input data length MUST be in correspondence with the TLV passed as the first parameter!
Returns
sl_tatus_t
esl_core_get_responses#
uint8_t esl_core_get_responses (uint8_t remaining_length, uint8_t * buf_p)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | remaining_length | size of data out buffer |
| uint8_t * | [out] | buf_p | pointer to data buffer to copy the responses into |
Copy all possible responses from internal circular buffer to a temporary linear buffer. Circular buffer drops the successfully read out data, while it might keep remaining responses which doesn't fit into the target buffer. Consistency of any response will be kept, that is, it might copy less data than the allowed maximum length passed as the first parameter, if there are responses left still in the internal circular buffer which otherwise wouldn't fit into the target buffer as a whole message. Returns
overall length of responses, might be 0 if there's no response
esl_sensor_init#
void esl_sensor_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ESL Tag sensor init function. ESL Core component will call this during the initialization of application. This call is hidden and happens automatically.
esl_sensor_read#
sl_status_t esl_sensor_read (uint8_t index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index |
Read interface (only) for ESL Sensor. Returns
sl_status_t SL_NOT_SUPPORTED if the ESL Sensor component is missing.
esl_sensor_get_count#
uint8_t esl_sensor_get_count (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Get ESL Tag Sensor count Returns
Number of available sensors
esl_display_create#
sl_status_t esl_display_create (uint16_t width, uint16_t height, esl_display_type_t type, esl_display_info_p * info)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | width | Display horizontal pixel count. |
| uint16_t | [in] | height | Display vertical pixel count. |
| esl_display_type_t | [in] | type | Display type defined in BT SIG Assigned Numbers. |
| esl_display_info_p * | [out] | info | esl_display_info_p type pointer to the newly created display info data. This value needs to pass to esl_display_add call, which has to follow the invocation of esl_display_create for any new display to be created, fully and properly. |
Create an ESL Tag display. Any display which a Tag wants to implement needs to becreated properly in the first place.
Returns
sl_status_t
esl_display_add#
sl_status_t esl_display_add (esl_display_info_p info, esl_va_method_p init_func, esl_va_method_p write_func)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| esl_display_info_p | [in] | info | esl_display_info_p type pointer, can be get by calling esl_display_create previously. |
| esl_va_method_p | [in] | init_func | esl_va_method_p type pointer to the low-level init function of the display driver. Driver implementation, however, it's up to the user to implement it properly - the only rule is to follow the interface specification defined by the esl_va_method_p type. If the 'init' method is not necessary for the given display, then a NULL pointer can be passed. |
| esl_va_method_p | [in] | write_func | esl_va_method_p type pointer to the low-level write function of the display driver. Has to be implemented by the users, and it's mandatory (can't be NULL). |
Add an ESL Tag display to the list of available displays after creation. Any display on a Tag can be only used after adding it to the list.
Returns
sl_status_t
esl_display_bt_on_event#
void esl_display_bt_on_event (sl_bt_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack. |
ESL display's bluetooth stack event handler. This one runs by the user implementation (usually in app.c) in parallel.
esl_display_set_image#
sl_status_t esl_display_set_image (uint8_t display_index, uint8_t image_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | display_index | Selects the display to show the image on. |
| uint8_t | [in] | image_index | Selects the image to be shown on the display. |
ESL Display: chose an image to show. Invokes the users write_func passed to esl_display_add as its 3rd parameter. Returns
sl_status_t
esl_display_get_width#
sl_status_t esl_display_get_width (uint8_t display_index, uint16_t * width)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | display_index | Selects the display to get the width of. |
| uint16_t * | [out] | width | Horizontal pixel count of the selected display. |
Display width getter. Returns
sl_status_t
esl_display_get_height#
sl_status_t esl_display_get_height (uint8_t display_index, uint16_t * height)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | display_index | Selects the display to get the height of. |
| uint16_t * | [out] | height | Vertical pixel count of the selected display. |
Display height getter Returns
sl_status_t
esl_display_get_type#
sl_status_t esl_display_get_type (uint8_t display_index, esl_display_type_t * type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | display_index | Selects the display to get the type of. |
| esl_display_type_t * | [out] | type | esl_display_type_t Display type defined in BT SIG. |
Display type getter. Returns
sl_status_t
esl_led_add#
sl_status_t esl_led_add (esl_led_type_t type, uint8_t red_value, uint8_t green_value, uint8_t blue_value)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| esl_led_type_t | [in] | type | Possible ESL LED type defined by ESL standard |
| uint8_t | [in] | red_value | ESL LED (initial, in case of sRGB type) red color value. |
| uint8_t | [in] | green_value | ESL LED (initial, if sRGB) green color value. |
| uint8_t | [in] | blue_value | ESL LED (initial, if sRGB) blue color value. |
Add an ESL Tag LED to the list of available LEDs after creation. Any LED on a Tag can be only used after adding it to the internal LED registry.
Returns
sl_status_t
esl_led_on#
sl_status_t esl_led_on (uint8_t led_index, esl_led_gamut_control_t gamut)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | led_index | |
| esl_led_gamut_control_t | N/A | gamut |
ESL Tag LED on function. Simple turn on function with given brightness and color values, to be implemented by end users. It's the users responsibility to actually turn given LED on with the given brightness and color parameters (if applicable) and the function shall return SL_STATUS_OK in case of success. Return SL_STATUS_FAIL on any other case (e.g. index out of bound, detectable HW error etc. Returns
sl_status_t
esl_led_off#
sl_status_t esl_led_off (uint8_t led_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | led_index |
ESL Tag LED off function. Simple turn off function, similar to sl_esl_led_on method except it omits the gamut parameter entirely. To be implemented by end users. It's the users responsibility to actually turn given LED off and the function shall return SL_STATUS_OK in case of success. Return SL_STATUS_FAIL on any other case (e.g. index out of bound, detectable HW error etc. Returns
sl_status_t
esl_led_create_color#
esl_led_gamut_control_t esl_led_create_color (uint8_t red_value, uint8_t green_value, uint8_t blue_value, uint8_t brightness)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | red_value | ESL LED red color level |
| uint8_t | [in] | green_value | ESL LED red color level |
| uint8_t | [in] | blue_value | ESL LED red color level |
| uint8_t | [in] | brightness | ESL LED red color level |
Assembly ESL Tag LED gamut value from input parameters for esl_led_gamut_control_t type Returns
esl_led_gamut_control_t Resulting ESL LED gamut value
esl_led_bt_on_event#
void esl_led_bt_on_event (sl_bt_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack. |
ESL LED's bluetooth stack event handler. This one runs by the user implementation (usually in app.c) in parallel.