Current status of Configuration Executor.
Public Attributes#
State of Configuration Executor.
uint16_t
Network key index of the executed configuration job
It is valid if the state is not BTMESH_CONF_EXEC_STATE_IDLE.
uint16_t
Destination node primary element address of executed configuration job
It is valid if the state is not BTMESH_CONF_EXEC_STATE_IDLE.
Public Attribute Documentation#
state#
btmesh_conf_executor_state_t btmesh_conf_executor_status_t::state
State of Configuration Executor.
enc_netkey_index#
uint16_t btmesh_conf_executor_status_t::enc_netkey_index
Network key index of the executed configuration job
It is valid if the state is not BTMESH_CONF_EXEC_STATE_IDLE.
server_address#
uint16_t btmesh_conf_executor_status_t::server_address
Destination node primary element address of executed configuration job
It is valid if the state is not BTMESH_CONF_EXEC_STATE_IDLE.