Bluetooth Mesh SDK Version 10.2.0 - Release Notes (May 4, 2026)#
Bluetooth Mesh is a standards-based, many-to-many communication topology available for Bluetooth Low Energy (LE) devices, optimized for large-scale networks and ideally suited for building automation, sensor networks, and asset tracking.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 10.2.0#
None.
Added in 10.1.0#
None.
Added in 10.0.0#
Added support for GCC LTO (Link-Time Optimization) to enable smaller firmware code size. Note that LTO is now the default choice for Bluetooth Mesh applications.
API Changes#
Changed in 10.2.0#
Added iterative API to query provisioning database entries.
Changed in 10.1.0#
Added API to control LC regulator operation.
Added API to set a timeout after which LC considers ambient light level input to be unavailable.
Changed in 10.0.0#
Relaxed LPN polling configuration parameters.
Added API call sl_btmesh_config_client_prepare_key_refresh(), replacing deprecated API call sl_btmesh_test_prov_prepare_key_refresh().
Added API call sl_btmesh_node_test_proxy_beacon().
Unnecessary configuration value SL_BTMESH_CONFIG_MAX_GATT_CONNECTIONS removed. The Bluetooth LE connection count configuration determines how many parallel Mesh GATT connections can be made use of.
Bug Fixes#
Fixed in 10.2.0#
Fixed an issue with emitting Config Node Reset Status message when a node is being reset.
Corrected a number of lighting and LC regulator related issues.
Fixed in 10.1.0#
Resolved firmware distribution issues to stem from misconfiguration, not a bug.
Fixed a group address parsing error in host Python code for OTA DFU.
Fixed in 10.0.0#
Removed unnecessary network key: application key bonding check when running a key refresh procedure at an embedded Provisioner.
Fixed SAR Segments Threshold state value use in transport layer.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 10.2.0#
None.
Added in 10.1.0#
None.
Added in 10.0.0#
Added support for GCC LTO (Link-Time Optimization) to enable smaller firmware code size. Whereas regular compiler optimization can only work on code one compilation unit at a time, LTO covers the whole of the firmware image to be built. This enables optimizations across compilation units and typically results in significant reduction to the firmware size, meaning that the saved flash area can be used for other purposes.
Enhancements#
Added in 10.2.0#
Provided an iterative API for querying the provisioning database entries on a provisioner one-by-one. This allows the application to exercise more fine-grained control on how it pulls in the DDB data.
Added in 10.1.0#
Improved the LC model API by allowing the configuration of the LC regulator to be enabled, disabled, or conditionally enabled depending on whether there is ambient light level input available or not. Related to the sensor input, the application can now set a configurable timeout; if no ambient light level input is received within the specified time, the input is considered to be not available.
Added in 10.0.0#
Relaxed the maximum values for limits after which an LPN considers a friendship stale. New limits allow for LPN to try 240 times to poll a friend at a maximum of 60 second intervals. This can be helpful to avoid re-establishing a friendship from scratch in case a Friend node is temporarily overloaded by other traffic.
Provided the key refresh customization API in the config client API class. This allows applications to avoid including the test API class while still allowing them to execute finely-tuned key refresh procedures.
Provided better functionality for checking GATT proxy service advertisements for known network and node identity validity, whether the advertisements are private or not.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 10.2.0#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
sl_status_t sl_btmesh_prov_get_ddb_entry_by_count | N/A |
sl_status_t sl_btmesh_prov_get_ddb_entry_count | N/A |
Added in 10.1.0#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
sl_status_t sl_btmesh_lc_server_set_regulator_mode | N/A |
sl_status_t sl_btmesh_lc_server_set_sensor_timeout | N/A |
Added in 10.0.0#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
sl_status_t sl_btmesh_node_test_proxy_beacon | N/A |
sl_status_t sl_btmesh_config_client_prepare_key_refresh |
Modified APIs#
Added in 10.2.0#
None.
Added in 10.1.0#
None.
Added in 10.0.0#
As a general note, API calls that do not take any parameters are now explicitly defined as such instead of having no parameter list, e.g., sl_status_t sl_btmesh_node_init(void) instead of sl_status_t sl_btmesh_node_init(). This should have no effect for correctly written applications.
Range of the LPN configuration setting sl_btmesh_lpn_request_retries has been increased from 0..10 to 0..239.
Range of the LPN configuration setting sl_btmesh_lpn_retry_interval has been increased from 0..100 ms to 0..60000 ms.
Removed APIs#
Removed in 10.2.0#
None.
Removed in 10.1.0#
None.
Removed in 10.0.0#
Removed API Name | Was Deprecated? |
|---|---|
SL_BTMESH_CONFIG_MAX_GATT_CONNECTIONS | No |
Deprecated APIs#
Deprecated in 10.2.0#
None.
Deprecated in 10.1.0#
None.
Deprecated in 10.0.0#
Deprecated API Name | Planned Removal Date |
|---|---|
Jun 2026 |
Bug Fixes#
Fixed in 10.2.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1565219 | Lightness value could roll over minimum/maximum value when using Generic Level move or halt requests | 00335738 | All; generic software issue |
| 1564592 | Switching a light off while dimming it did not work as expected. | 00335024 | All; generic software issue |
| 1565493 | A potential race condition existed between LC regulator adjusting light level and user manually dimming up or down. | 00335738 | All; generic software issue |
| 1576029 | Fixed an issue with user controlling LC Mode manually. | 00338266 | All; generic software issue |
| 1621791 | Config Node Reset Status message might remain unsent at node reset due to encryption keys being deleted before the message was encrypted. Delayed key removal slightly to allow for message construction to happen first. | 00340071 | All; generic software issue |
Fixed in 10.1.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1565037 | Resolved issues with firmware distribution failures in a large network that has a high proportion of relay nodes to be caused by misconfiguration, not a bug. | None | All; generic software issue |
| 1566633 | Fixed a group address parsing error in host Python code for OTA DFU. | None | All; generic software issue |
Fixed in 10.0.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1187276 | Removed unnecessary network key - application key bonding check when running a key refresh procedure at an embedded Provisioner. Key bindings on a node may differ from key bindings on the Provisioner, so a check is not useful. | None | All; generic software issue |
| 1485698 | Fixed SAR Segments Threshold state value use in transport layer. The state values were configurable but not used properly with segmented message communications. | None | All; generic software issue |
Chip Enablement#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
Added in 10.2.0#
None.
Added in 10.1.0#
None.
Added in 10.0.0#
| Example Name | Description | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Bluetooth Mesh - SoC Empty with Common Manufacturing Token Support. |
Demonstrates the bare minimum needed for a Bluetooth Mesh C application. The application sets its UUID and OOB provisioning capabilities depending on the manufacturing token used. The application also demonstrates how to use PSA crypto to validate the token signature. | Standard | SoC |
|
None |
|
Bluetooth Mesh - SoC DFU Target. |
Demonstrates the Firmware Update Target role defined in the Mesh Device Firmware Update Model specification. Target node receives firmware image from a Standalone Updater or Distributor node and applies the firmware image. | Standard | SoC |
|
None |
|
Bootloader - SoC Bluetooth AppLoader OTA DFU Non-Secure part of Bootloader using TrustZone. |
TrustZone is used to split into a Secure and Non-Secure bootloader. This is the non-secure part of the bootloader. The secure part of the bootloader, which contains the core functionalities needed to be built separately and used together with the non-secure part of the bootloader. | Standard | SoC |
|
None |
|
Bootloader - SoC Bluetooth AppLoader OTA DFU Secure part of Bootloader using TrustZone. |
TrustZone is used to split into a Secure and Non-Secure bootloader. This is the secure part of the bootloader. The non-secure part of the bootloader, which contains the communication interfaces needed to be built separately and used together with the secure part of the bootloader. | Standard | SoC |
|
None |
|
Bootloader - SoC Internal Storage (Bluetooth Mesh) |
This sample configuration of the Gecko bootloader configures the bootloader to use the internal main flash to store firmware update images. The storage configuration is set up to store a single firmware update image at a time, in a single storage slot. This can be configured on the "Storage" tab. | Standard | SoC |
|
None |
|
Bootloader - SoC SPI Flash Storage (single image for Bluetooth Mesh) |
This sample configuration of the Gecko bootloader configures the bootloader to use an external SPI flash to store firmware update images. The storage configuration is set up to store a single firmware update image at a time, in a single storage slot. The storage slot is configured to start at address 0x0 of the SPI flash, and have a size of 1 MB. This can be configured on the "Storage" tab. | Standard | SoC |
|
None |
Modified Examples#
Modified in 10.2.0#
None.
Modified in 10.1.0#
None.
Modified in 10.0.0#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Bluetooth Mesh - SoC DFU Distributor |
A workspace was provided to associate a bootloader with the project. | N/A | SoC |
|
N/A |
| All embedded examples except: Bluetooth Mesh - SoC DFU Target, Bluetooth Mesh - SoC DFU Distributor, Bluetooth Mesh - SoC Empty with Certificate-Based Provisioning support |
|
Standard | SoC |
|
N/A |
| All host examples |
|
Standard | NCP Host |
|
UART |
Removed Examples#
None.
Deprecated Examples#
Deprecated in 10.2.0#
None.
Deprecated in 10.1.0#
None.
Deprecated in 10.0.0#
Btmesh_soc_tz_secure_application, btmesh_soc_empty_cbp_tz, and btmesh_soc_csr_generator_tz will disappear as standalone examples as they are to be used from their respective slcw workspaces instead.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 401550 | No BGAPI event for segmented message handling failure. | 212392, 214429, 216665 | Application needs to deduce failure from timeout / lack of application layer response; for vendor models, an API has been provided. | All; generic software issue |
| 454059 | A large number of key refresh state change events are generated at the end of KR process, and that may flood NCP queue. | None | Increase NCP queue length in the project. | NCP interface; generic software issue |
| 454061 | Slight performance degradation compared to 1.5 in round-trip latency tests was observed. | None | None | All; generic software issue |
| 624514 | Issue with re-establishing connectable advertising if all connections have been active and GATT proxy is in use. | 235615 | Allocate one more connection than is needed. | All; generic software issue |
| 841360 | Poor performance of segmented message transmission over GATT bearer. | 283876 | Ensure that the underlying BLE connection’s Connection interval is short; ensure that ATT MTU is large enough to fit a full Mesh PDU; tune the minimum connection event length to allow multiple LL packets to be transmitted per connection event. | All; generic software issue |
| 1204017 | Distributor is not able to handle parallel self FW Update and FW Upload. | None | Don’t run self FW update and FW upload in parallel. | All; generic software issue |
| 1226127 | Host provisioner example can be stuck when it starts to provision a second node. | None | Restart the host provisioner app before provisioning the second node. | All; generic software issue |