Bluetooth Mesh Proxy Connections#
Bluetooth Mesh Proxy Connections.
Bluetooth mesh stack functions for GATT proxy connections
Modules#
sl_btmesh_evt_proxy_disconnected
sl_btmesh_evt_proxy_filter_status
Functions#
Macros#
Function Documentation#
sl_btmesh_proxy_connect#
sl_status_t sl_btmesh_proxy_connect (uint8_t connection, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | connection | Connection handle |
| uint32_t * | [out] | handle | If a connection attempt is successfully initiated, a valid proxy handle will be returned. |
Start connecting a proxy client to a proxy server. After the connection is complete, a sl_btmesh_evt_proxy_connected event will be generated. LE-connection must be opened prior to opening the proxy connection.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_proxy_disconnect#
sl_status_t sl_btmesh_proxy_disconnect (uint32_t handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | handle | Proxy handle |
Disconnect. This call can be used also for a connection, which is not yet fully formed.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_proxy_set_filter_type#
sl_status_t sl_btmesh_proxy_set_filter_type (uint32_t handle, uint16_t netkey_index, uint8_t type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | handle | Proxy handle |
| uint16_t | [in] | netkey_index | Network key index used in encrypting the request to the proxy server |
| uint8_t | [in] | type | Filter type: 0x00 to allow traffic from the given address, 0x01 to block traffic from the given address |
Set up the proxy filtering type. At the proxy server side, this is a local configuration, while on the proxy client a proxy configuration PDU will be sent to the proxy server.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_proxy_allow#
sl_status_t sl_btmesh_proxy_allow (uint32_t handle, uint16_t netkey_index, uint16_t address)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | handle | Proxy handle |
| uint16_t | [in] | netkey_index | Network key index used in encrypting the request to the proxy server |
| uint16_t | [in] | address | Destination address to allow. The address may be either a unicast address, a group address, or a virtual address. |
Allow messages meant for the given address to be forwarded over the proxy connection to the proxy client. At the proxy server side, this is a local configuration, while on the proxy client a proxy configuration PDU will be sent to the proxy server.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_proxy_deny#
sl_status_t sl_btmesh_proxy_deny (uint32_t handle, uint16_t netkey_index, uint16_t address)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | handle | Proxy handle |
| uint16_t | [in] | netkey_index | Network key index used in encrypting the request to the proxy server |
| uint16_t | [in] | address | Destination address to block. The address may be either a unicast address, a group address, or a virtual address. |
Block messages meant for the given address from being forwarded over the proxy connection to the proxy client. At the proxy server side, this is a local configuration, while on the proxy client a proxy configuration PDU will be sent to the proxy server.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_proxy_optimisation_toggle#
sl_status_t sl_btmesh_proxy_optimisation_toggle (uint8_t enable)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | enable | Non zero - enable, otherwise disable |
In case of unicast address, if proxy identified the destination, the message will be forwarded only to that node, otherwise to all. This functionality could be enabled or disabled with this function.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_proxy_send_solicitation#
sl_status_t sl_btmesh_proxy_send_solicitation (uint8_t enc_netkey_index, uint16_t elem_index, uint16_t dst)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | enc_netkey_index | Network key index used to encrypt the message |
| uint16_t | [in] | elem_index | Solicitation source element index. Proxy client may use the primary address of any of the secondary addresses as a solicitation source |
| uint16_t | [in] | dst | Solicitation destination address. Solicitation does not have a subscribe mechanism, the address can be the primary or any of the secondary addresses. In addition, 0xFFFC (All Proxies) is permitted |
Send Solicitation PDU to activate a Private Proxy on a node that support On-Demand Private Proxy.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Macro Definition Documentation#
sl_btmesh_cmd_proxy_set_filter_type_id#
#define sl_btmesh_cmd_proxy_set_filter_type_idValue:
0x02180028
sl_btmesh_cmd_proxy_optimisation_toggle_id#
#define sl_btmesh_cmd_proxy_optimisation_toggle_idValue:
0x05180028
sl_btmesh_cmd_proxy_send_solicitation_id#
#define sl_btmesh_cmd_proxy_send_solicitation_idValue:
0x06180028
sl_btmesh_rsp_proxy_set_filter_type_id#
#define sl_btmesh_rsp_proxy_set_filter_type_idValue:
0x02180028
sl_btmesh_rsp_proxy_optimisation_toggle_id#
#define sl_btmesh_rsp_proxy_optimisation_toggle_idValue:
0x05180028
sl_btmesh_rsp_proxy_send_solicitation_id#
#define sl_btmesh_rsp_proxy_send_solicitation_idValue:
0x06180028