Lightness Server#

Used to support the control and reporting functionality of a node with a light source that is dimmable. Lightness Server extends Generic Power OnOff Server model and Generic Level Server model. It also has a corresponding Lightness Setup Server model which is present in the same element. The component provides the reporting functions, and the possibility to set current, default, and last values of the lightness value. This component is prepared for integration into SOC applications. This is a Low-Code component. The following weak callback is available to implement the relevant light source handling: void sl_btmesh_lighting_level_pwm_cb(uint16_t level);

Functions#

void
sl_btmesh_lighting_set_level(uint16_t level, uint32_t transition_ms)
void
uint16_t
void
sl_btmesh_lighting_server_on_ui_update(uint16_t lightness_level)
sl_status_t

Stop the lighting level transition timer.

void
void
void
sl_btmesh_set_lightness_target(uint16_t lightness)
void
void
sl_btmesh_set_lightness_last(uint16_t lightness)
void
sl_btmesh_update_lightness(uint16_t lightness, uint32_t remaining_ms)

Macros#

#define

light off (both LEDs turned off)

#define

light on (both LEDs turned on)

#define

provisioning (LEDs blinking)

Function Documentation#

sl_btmesh_lighting_set_level#

void sl_btmesh_lighting_set_level (uint16_t level, uint32_t transition_ms)
Parameters
TypeDirectionArgument NameDescription
uint16_tN/Alevel
uint32_tN/Atransition_ms

sl_btmesh_set_state#

void sl_btmesh_set_state (int state)
Parameters
TypeDirectionArgument NameDescription
intN/Astate

sl_btmesh_get_level#

uint16_t sl_btmesh_get_level (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_btmesh_lighting_level_pwm_cb#

void sl_btmesh_lighting_level_pwm_cb (uint16_t level)
Parameters
TypeDirectionArgument NameDescription
uint16_tN/Alevel

sl_btmesh_lighting_server_on_ui_update#

void sl_btmesh_lighting_server_on_ui_update (uint16_t lightness_level)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]lightness_level

lightness level (0x0001 - FFFE)

Called when the UI shall be updated with the changed state of lightning server during a transition. The rate of this callback can be controlled by changing the SL_BTMESH_LIGHTING_SERVER_UI_UPDATE_PERIOD_CFG_VAL macro.

This is a callback which can be implemented in the application. Note

  • If no implementation is provided in the application, then the default weak implementation will be an empty function.


sl_btmesh_stop_transition_timer#

sl_status_t sl_btmesh_stop_transition_timer (void )

Stop the lighting level transition timer.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status code indicating success or error.


sl_btmesh_lighting_server_init#

void sl_btmesh_lighting_server_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Lighting Server initialization. This should be called at each boot if provisioning is already done. Otherwise this function should be called after provisioning is completed. This function is called automatically after enabling the component.


sl_btmesh_lighting_server_on_event#

void sl_btmesh_lighting_server_on_event (sl_btmesh_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_btmesh_msg_t *[in]evt

Pointer to incoming event.

Handling of mesh lighting server events.

This function is called automatically after enabling the component.


sl_btmesh_lighting_server_on_node_reset#

void sl_btmesh_lighting_server_on_node_reset (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Handle node reset.

Function for clearing component specific nvm content during node reset. This function is called automatically by Universal Configurator after enabling the component.


sl_btmesh_get_lightness_current#

uint16_t sl_btmesh_get_lightness_current (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get current lightness value

Returns

  • Current lightness


sl_btmesh_set_lightness_current#

void sl_btmesh_set_lightness_current (uint16_t lightness)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]lightness

Current lightness

Set current lightness value


sl_btmesh_get_lightness_target#

uint16_t sl_btmesh_get_lightness_target (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get target lightness value

Returns

  • Target lightness


sl_btmesh_set_lightness_target#

void sl_btmesh_set_lightness_target (uint16_t lightness)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]lightness

Target lightness

Set target lightness value


sl_btmesh_get_lightness_default#

uint16_t sl_btmesh_get_lightness_default (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get default lightness value

Returns

  • Default lightness


sl_btmesh_set_lightness_default#

void sl_btmesh_set_lightness_default (uint16_t lightness)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]lightness

Default lightness

Set default lightness value


sl_btmesh_set_lightness_last#

void sl_btmesh_set_lightness_last (uint16_t lightness)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]lightness

Last lightness

Set last lightness value


sl_btmesh_get_default_transition_time#

uint32_t sl_btmesh_get_default_transition_time (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

This function converts mesh format of default transition time to milliseconds.

Returns

  • Default transition time in milliseconds.


sl_btmesh_get_lightness_onpowerup#

uint8_t sl_btmesh_get_lightness_onpowerup (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get default lightness value on power up

Returns

  • Default lightness on power up


sl_btmesh_update_lightness#

void sl_btmesh_update_lightness (uint16_t lightness, uint32_t remaining_ms)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]lightness

Current lightness level within the transition

uint32_t[in]remaining_ms

Remaining transition time in milliseconds

This function updates the lightness level in the mesh stack during a transition


pri_level_move_stop#

void pri_level_move_stop (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

This function stops generic level move on primary element.


Macro Definition Documentation#

LED_STATE_OFF#

#define LED_STATE_OFF
Value:
0

light off (both LEDs turned off)


LED_STATE_ON#

#define LED_STATE_ON
Value:
1

light on (both LEDs turned on)


LED_STATE_PROV#

#define LED_STATE_PROV
Value:
2

provisioning (LEDs blinking)