Btmesh Provisioner#
This component automatically initializes the device as a provisioner on boot event. This component is prepared for integration into SOC applications. This is a No-Code component.
Functions#
void
sl_btmesh_provisioner_on_init(sl_status_t result)
void
sl_bt_provisioner_on_event(sl_bt_msg_t *evt)
Function Documentation#
sl_btmesh_provisioner_on_init#
void sl_btmesh_provisioner_on_init (sl_status_t result)
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_status_t | [in] | result | return value of the function call |
This function is called after the sl_btmesh_prov_init() function.
This is a callback which can be implemented in the application. Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_bt_provisioner_on_event#
void sl_bt_provisioner_on_event (sl_bt_msg_t * evt)
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_bt_msg_t * | [in] | evt | Pointer to incoming event. |
Handle BLE events for the provisioner.
This function is called automatically after enabling the component.