Scene Client#

Used to support the functionality of a node that can configure scenes on a network and trigger a state transition to a scene on another node. This component provides a function to recall a scene identified by its number. This component is prepared for integration into SOC applications. This is a No-Code component, if it is used with other compatible software components (eg.: CTL client).

Functions#

void
sl_btmesh_select_scene(uint8_t scene_to_recall)
void

Function Documentation#

sl_btmesh_select_scene#

void sl_btmesh_select_scene (uint8_t scene_to_recall)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]scene_to_recall

Scene to recall, possible values 1-255.

This function select scene and send it to the server.


sl_btmesh_handle_scene_client_on_event#

void sl_btmesh_handle_scene_client_on_event (sl_btmesh_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_btmesh_msg_t *[in]evt

Pointer to incoming event.

Handle Sensor Server events.

This function is called automatically after enabling the component.