BLOB Transfer progress
This structure represent the progress of the active BLOB Transfer Servers
Note
Some servers could fail with error or timeout, but if there is at least one active BLOB Transfer Server then the transfer continues
Public Attribute Documentation#
confirmed_tx_bytes#
uint32_t sl_btmesh_blob_transfer_client_progress_t::confirmed_tx_bytes
Number of BLOB bytes which have been received by every active BLOB Transfer Server
Note
The progress is calculated at the end of the blocks because in the block, chunks could be retransmitted multiple times