Advertisement Extension Server#
Advertisement Extension Server component enables the Silabs Configuration Server vendor model for the node to allow data transfer over Advertisement Extension. This is a proprietary feature which breaks compliance with AE in BT Mesh 1.1 specification. Mesh data over Advertisement Extension can be used in message-heavy applications (e.g. Device Firmware Update) to speed up data transfer between nodes. All nodes must have the Silabs Configuration Server vendor model enabled, and a Silabs Configuration Client (enabled by e.g. the Advertisement Extension Client component) must configure the clients to use Advertisement Extension. This component is prepared for integration into SOC applications. This is a No-Code component.
Functions#
Function Documentation#
sl_btmesh_ae_server_on_event#
void sl_btmesh_ae_server_on_event (const sl_btmesh_msg_t *const evt)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| const sl_btmesh_msg_t *const | [in] | evt | Pointer to incoming event.  | 
Handle Advertisement Extension Server events.
This function is called automatically after enabling the component.