CTL Server#
Color Tunable Lighting (CTL) Server model. Used to support the control and reporting functionality of a node with a light source that is dimmable and whose color temperature can be selected. This component implements this control and reporting functionality, extending on lighting server, and also provides callbacks on lighting related events. For more details about lighting, please see Lighting Server. This component is prepared for integration into SOC applications. This is a Low-Code component. The following weak callbacks are available to implement the relevant light source handling: void sl_btmesh_lighting_level_pwm_cb(uint16_t level); void sl_btmesh_lighting_color_pwm_cb(uint16_t color);
Functions#
Function Documentation#
sl_btmesh_ctl_server_on_event#
void sl_btmesh_ctl_server_on_event (sl_btmesh_msg_t * evt)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_btmesh_msg_t * | [in] | evt | Pointer to incoming event.  | 
Handle CTL Server events.
This function is called automatically after enabling the component.
sl_btmesh_ctl_server_init#
void sl_btmesh_ctl_server_init (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
CTL Server initialization. This should be called at each boot if provisioning is already done. Otherwise this function should be called after provisioning is completed. This function is called automatically after enabling the component.
sl_btmesh_ctl_server_on_node_reset#
void sl_btmesh_ctl_server_on_node_reset (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Component node reset handler. Clearing component specific nvm content during node reset. This function is called automatically by Universal Configurator after enabling the component.
sl_btmesh_get_temperature#
uint16_t sl_btmesh_get_temperature (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Function for retrieving actual temperature.
Returns
Actual temperature level.
sl_btmesh_get_deltauv#
uint16_t sl_btmesh_get_deltauv (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Function for retrieving actual delta UV.
Returns
Actual delta UV level.
sl_btmesh_ctl_set_temperature_deltauv_level#
void sl_btmesh_ctl_set_temperature_deltauv_level (uint16_t temperature, int16_t deltauv, uint32_t transition_ms)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | temperature | Temperature of color.  | 
| int16_t | [in] | deltauv | Delta UV value.  | 
| uint32_t | [in] | transition_ms | Transition time in milliseconds.  | 
Set LED temperature and delta UV in given transition time.
sl_btmesh_ctl_server_snprint_deltauv#
int sl_btmesh_ctl_server_snprint_deltauv (char * buffer, uint16_t buffer_size, uint16_t deltauv_raw)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| char * | [out] | buffer | Character buffer where the formatted delta UV is stored  | 
| uint16_t | [in] | buffer_size | Size of the character buffer  | 
| uint16_t | [in] | deltauv_raw | Raw value of the Delta UV CTL parameter  | 
Utility function to print the delta UV raw value into the passed character buffer in the <sign>X.XX format.
Returns
same as snprintf
sl_btmesh_lighting_color_pwm_cb#
void sl_btmesh_lighting_color_pwm_cb (uint16_t color)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | color | Desired light color PWM level.  | 
Callback for setting Light Color by PWM level (0x0001 - FFFE)
sl_btmesh_ctl_on_ui_update#
void sl_btmesh_ctl_on_ui_update (uint16_t temperature, uint16_t deltauv)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | temperature | Temperature of color.  | 
| uint16_t | [in] | deltauv | Delta UV value.  | 
Called when the UI shall be updated with the changed CTL Model state during a transition. The rate of this callback can be controlled by changing the SL_BTMESH_CTL_SERVER_UI_UPDATE_PERIOD_CFG_VAL macro.
This is a callback which can be implemented in the application. Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.