Firmware Update Client#
Provides BT Mesh Firmware Update Client functionality, defined in mesh specification. The Firmware Update Client model is used by the Distributor and Initiator. This component is prepared for integration into SOC applications. The Initiator uses this model to retrieve the information about the firmware subsystems installed on the Target node, and to get the location of the new firmware images. The Initiator receives the list of Target nodes from the higher-layer application. The Distributor uses this model to start a firmware image transfer to the Target nodes. The Distributor receives the list of Target nodes from the Initiator. The Distributor uses the procedures on the Firmware Update Client model with the inputs to these procedures being chosen by the Firmware Distribution Server. This is a No-Code component.
Functions#
Function Documentation#
sl_btmesh_firmware_update_client_on_event#
void sl_btmesh_firmware_update_client_on_event (const sl_btmesh_msg_t *const evt)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| const sl_btmesh_msg_t *const | [in] | evt | Pointer to incoming event.  | 
Handle Firmware Update Client events.
This function is called automatically after enabling the component.