Bluetooth Mesh Remote Provisioning#
NOTE: This section replaces AN1368: Bluetooth Mesh Remote Provisioning. Further updates to this application note will be provided here.
This application note describes the Mesh Remote Provisioning feature. Without it, the provisioner and the unprovisioned node must be in radio range of each other. With it, a device can be provisioned without a direct radio connection between the provisioner and the unprovisioned node. The feature uses standard Mesh networking between the provisioner and a Remote Provisioning Server, so that the server can provision any device in the radio range of the network.
Key Points#
Remote Provisioning Background information
Remote Provisioning in Bluetooth Mesh SDK
Bluetooth Mesh Example Applications
Remote Provisioning Example Walkthrough