BLOB Storage#
Provides an API for storing binary large objects (BLOB) via the bootloader. The number and size of the bootloader slots determines the number and maximum size of BLOBs that can be stored on the device. Please check the bootloader configuration. This component is prepared for integration into SOC applications. This is a No-Code component, if it is used with either BLOB transfer Client or Server components.
Modules#
sl_btmesh_blob_storage_slot_metadata_cache_t
Enumerations#
Typedefs#
Functions#
Macros#
Reserved BLOB Storage owner ID of FW Distribution Server.
Reserved BLOB Storage app ID of Firmware ID (BT Mesh DFU)
Reserved BLOB Storage app ID of Metadata (BT Mesh DFU)
Reserved BLOB Storage app ID of managed flag.
Enumeration Documentation#
sl_btmesh_blob_storage_status_e#
sl_btmesh_blob_storage_status_e
| Enumerator | |
|---|---|
| SL_BTMESH_BLOB_STORAGE_STATUS_EMPTY | Slot is empty. |
| SL_BTMESH_BLOB_STORAGE_STATUS_CORRUPTED | Slot data is corrupted
|
| SL_BTMESH_BLOB_STORAGE_STATUS_INVALIDATED | Slot has valid data but footer was invalidated by application. |
| SL_BTMESH_BLOB_STORAGE_STATUS_OCCUPIED | Slot has data and is valid. |
| SL_BTMESH_BLOB_STORAGE_STATUS_INTERNAL_ERROR | Internal API error. |
sl_btmesh_blob_storage_delete_state_e#
sl_btmesh_blob_storage_delete_state_e
| Enumerator | |
|---|---|
| SL_BTMESH_BLOB_STORAGE_DELETE_INACTIVE | Asynchronous delete inactive. |
| SL_BTMESH_BLOB_STORAGE_DELETE_BUSY | Asynchronous delete active and busy. |
| SL_BTMESH_BLOB_STORAGE_DELETE_FAILED | Asynchronous delete has failed. |
| SL_BTMESH_BLOB_STORAGE_DELETE_SUCCESS | Asynchronous delete has succeeded. |
Typedef Documentation#
sl_btmesh_blob_storage_status_t#
typedef enum sl_btmesh_blob_storage_status_e sl_btmesh_blob_storage_status_t
sl_btmesh_blob_storage_delete_state_t#
typedef enum sl_btmesh_blob_storage_delete_state_e sl_btmesh_blob_storage_delete_state_t
Function Documentation#
sl_btmesh_blob_storage_init#
void sl_btmesh_blob_storage_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initializes the storage wrapper
sl_btmesh_blob_storage_deinit#
void sl_btmesh_blob_storage_deinit (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Deinitializes the storage wrapper
sl_btmesh_blob_storage_read#
sl_status_t sl_btmesh_blob_storage_read (sl_bt_uuid_64_t const * blob_id, uint32_t offset, uint32_t * len, void * buffer)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
| uint32_t | [in] | offset | Offset relative to BLOB start, where read should start |
| uint32_t * | [inout] | len | Length of the buffer; modified if there's less data then buffer could fit |
| void * | [out] | buffer | Buffer in which data is read |
Reads data from the identified BLOB into a buffer
Returns
Status code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: In case BLOB isn't found
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_write_start#
sl_status_t sl_btmesh_blob_storage_write_start (sl_bt_uuid_64_t const * blob_id, uint32_t size)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB about to be written into storage |
| uint32_t | [in] | size | Size of the BLOB about to be written into storage |
Starts writing procedure
Sets internal state variables to correspond to writing a BLOB. Returns
Status code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_ALREADY_EXISTS: In case BLOB ID already exists in storage
SL_STATUS_WOULD_OVERFLOW: In case BLOB is too big to fit
SL_STATUS_NO_MORE_RESOURCE: In case no slot is available
SL_STATUS_BUSY: In case BLOB Storage is processing an async. request
sl_btmesh_blob_storage_write#
sl_status_t sl_btmesh_blob_storage_write (uint32_t offset, uint32_t len, void * data)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | offset | Offset of the data inside the BLOB. Must be |
| uint32_t | [in] | len | Length of the data |
| void * | [in] | data | Pointer to the data |
Writes data into storage.
sl_btmesh_blob_storage_write_start must be called first.
Returns
Result of write operation
Return values
SL_STATUS_OK: In case of success
SL_STATUS_FLASH_WRITE_INHIBITED: In case of non-word aligned offset
SL_STATUS_FLASH_PROGRAM_FAILED: In case storage programming failed
sl_btmesh_blob_storage_get_cache#
void sl_btmesh_blob_storage_get_cache (sl_btmesh_blob_storage_slot_metadata_cache_t const ** cache, uint32_t * len)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_blob_storage_slot_metadata_cache_t const ** | [out] | cache | Pointer to the buffer of a pointer for cache start |
| uint32_t * | [out] | len | Pointer to the length cache |
Retrieves a pointer to the cache
sl_btmesh_blob_storage_any_blob_corrupted#
bool sl_btmesh_blob_storage_any_blob_corrupted (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns if any BLOB is corrupted
Returns
Return values
true: If at least one BLOB is corrupted
false: If no BLOB is corrupted
sl_btmesh_blob_storage_verify#
sl_status_t sl_btmesh_blob_storage_verify (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Verifies the BLOB to be considered consistent
Returns
Verification result
Return values
SL_STATUS_OK: In case of success
SL_STATUS_INVALID_STATE: In case less data has been written than indicated with
SL_STATUS_FAIL: In case of internal API error
SL_STATUS_FLASH_PROGRAM_FAILED: In case writing validity info into storage has failed
sl_btmesh_blob_storage_invalidate#
sl_status_t sl_btmesh_blob_storage_invalidate (sl_bt_uuid_64_t const * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB to invalidate |
Invalidates BLOB footer
Returns
Result code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: In case BLOB identifier is not found
SL_STATUS_FAIL: In case of internal API error
SL_STATUS_FLASH_PROGRAM_FAILED: In case storage writing has failed
SL_STATUS_BUSY: In case BLOB Storage is processing an async. request
sl_btmesh_blob_storage_invalidate_by_owner#
sl_status_t sl_btmesh_blob_storage_invalidate_by_owner (uint16_t owner_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | owner_id | Identifier of owner |
Invalidates all valid BLOB footer which belongs to a specific owner
See Also
Returns
Result code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_FAIL: In case of internal API error
SL_STATUS_FLASH_PROGRAM_FAILED: In case storage writing has failed
SL_STATUS_BUSY: In case BLOB Storage is processing an async. request
sl_btmesh_blob_storage_invalidate_all#
sl_status_t sl_btmesh_blob_storage_invalidate_all (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Invalidates all valid BLOB footer
Returns
Result code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_FAIL: In case of internal API error
SL_STATUS_FLASH_PROGRAM_FAILED: In case storage writing has failed
SL_STATUS_BUSY: In case BLOB Storage is processing an async. request
sl_btmesh_blob_storage_delete#
sl_status_t sl_btmesh_blob_storage_delete (sl_bt_uuid_64_t const * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB to be deleted |
Deletes a BLOB from storage
Returns
Result of erase
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: In case no BLOB has been identified in storage
SL_STATUS_FLASH_ERASE_FAILED: In case erase has failed
sl_btmesh_blob_storage_delete_start#
sl_status_t sl_btmesh_blob_storage_delete_start (sl_bt_uuid_64_t const * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB to be deleted |
Start asynchronous delete of a BLOB
See Also
Returns
Request status
Return values
SL_BTMESH_OK: Request successful
SL_BTMESH_BUSY: Erase handler busy
sl_btmesh_blob_storage_delete_managed_by_owner#
sl_status_t sl_btmesh_blob_storage_delete_managed_by_owner (uint16_t owner_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | owner_id | Identifier of owner |
Deletes all BLOB from storage which belongs to a specific owner
See Also
Returns
Result of erase
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: No managed slot was found which belongs to the owner
SL_STATUS_FLASH_ERASE_FAILED: In case erase has failed
sl_btmesh_blob_storage_delete_managed_by_owner_start#
sl_status_t sl_btmesh_blob_storage_delete_managed_by_owner_start (uint16_t owner_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | owner_id | Identifier of owner |
Start asynchronous delete of BLOBs that are unmanaged
See Also
Returns
Request status
Return values
SL_BTMESH_OK: Request successful
SL_BTMESH_BUSY: Erase handler busy
sl_btmesh_blob_storage_delete_all#
sl_status_t sl_btmesh_blob_storage_delete_all (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Deletes all BLOBs from storage
Returns
Result of erase
Return values
SL_STATUS_OK: In case of success
SL_STATUS_FLASH_ERASE_FAILED: In case erase has failed
sl_btmesh_blob_storage_delete_all_start#
sl_status_t sl_btmesh_blob_storage_delete_all_start (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Start asynchronous delete of all BLOBs
See Also
Returns
Request status
Return values
SL_BTMESH_OK: Request successful
SL_BTMESH_BUSY: Erase handler busy
sl_btmesh_blob_storage_delete_invalid_slots#
sl_status_t sl_btmesh_blob_storage_delete_invalid_slots (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Clear slots with invalid data
Returns
Result of erase
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: No invalid slot was found
SL_STATUS_FLASH_ERASE_FAILED: In case erase has failed
sl_btmesh_blob_storage_delete_invalid_slots_start#
sl_status_t sl_btmesh_blob_storage_delete_invalid_slots_start (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Start asynchronous delete of invalid BLOBs
See Also
Returns
Request status
Return values
SL_BTMESH_OK: Request successful
SL_BTMESH_BUSY: Erase handler busy
sl_btmesh_blob_storage_delete_unmanaged_slots#
sl_status_t sl_btmesh_blob_storage_delete_unmanaged_slots (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Clear slots that are unmanaged
See Also
Returns
Result of erase
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: No unmanaged slot was found
SL_STATUS_FLASH_ERASE_FAILED: In case erase has failed
sl_btmesh_blob_storage_delete_unmanaged_slots_start#
sl_status_t sl_btmesh_blob_storage_delete_unmanaged_slots_start (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Start asynchronous delete of BLOBs that are unmanaged
See Also
Returns
Request status
Return values
SL_BTMESH_OK: Request successful
SL_BTMESH_BUSY: Erase handler busy
sl_btmesh_blob_storage_set_delete_separation_time#
sl_status_t sl_btmesh_blob_storage_set_delete_separation_time (uint16_t separation_time_ms)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | separation_time_ms | Separation time between two async erase steps |
Set asynchronous delete separation time
Asynchronous delete separation time is measured in milliseconds between two asynchronous delete steps. The BLOB storage async delete is performed in multiple steps and each delete step blocks the code execution. If delete steps are executed too often then it could starve other timing sensitive SW components so delete separation time feature can be used to prevent this scenario.
Returns
Request status
Return values
SL_STATUS_OK: In case of success
sl_btmesh_blob_storage_is_present#
bool sl_btmesh_blob_storage_is_present (sl_bt_uuid_64_t const * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB inquired about |
Checks whether BLOB identified is present in storage
Returns
Boolean value
Return values
true: BLOB is present
false: BLOB is not present
sl_btmesh_blob_storage_get_blob_size#
sl_status_t sl_btmesh_blob_storage_get_blob_size (sl_bt_uuid_64_t const * blob_id, uint32_t * blob_size)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB inquired about |
| uint32_t * | [out] | blob_size | Length of the BLOB |
Queries the BLOB size
Returns
Status code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: In case no BLOB has been identified
sl_btmesh_blob_storage_calc_app_footer_size
uint32_t sl_btmesh_blob_storage_calc_app_footer_size (uint16_t footer_data_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | footer_data_length | Length of the application specific footer data |
Calculates the size of application specific footer on BLOB storage medium.
Note
BLOB storage stores some additional metadata (id, length) with the footer data and it takes into consideration the alignment requirements of the underlying medium.
Returns
Size of application specific footer on BLOB storage medium.
sl_btmesh_blob_storage_write_app_footer
sl_status_t sl_btmesh_blob_storage_write_app_footer (sl_bt_uuid_64_t const * blob_id, void const * footer, uint16_t app_id, uint16_t length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
| void const * | [in] | footer | Footer data |
| uint16_t | [in] | app_id | Identifier of the application data. Must be unique to the application layer user in the compiled software. Used to identify footer. |
| uint16_t | [in] | length | Length of the data |
Writes application specific footer into storage belonging to identified the BLOB and application
Returns
Result of app footer write
Return values
SL_STATUS_OK: In case of success
SL_STATUS_INVALID_PARAMETER: If app_id or length is invalid
SL_STATUS_FLASH_PROGRAM_FAILED: In case write failed
SL_STATUS_FULL: If there is no free space for app footer
SL_STATUS_NOT_FOUND: If blob_id doesn't identify any footer
SL_STATUS_INVALID_SIGNATURE: If any footer is corrupted during search for empty space to write new app footer
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_get_app_footer_length
sl_status_t sl_btmesh_blob_storage_get_app_footer_length (sl_bt_uuid_64_t const * blob_id, uint16_t app_id, uint16_t * length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
| uint16_t | [in] | app_id | Identifier of the application data |
| uint16_t * | [out] | length | Length of application data in case of success |
Queries footer information length assigned to a given BLOB, belonging to an application identifier.
Returns
Status code
Return values
SL_STATUS_OK: In case of successful query
SL_STATUS_NOT_FOUND: If app_id and blob_id don't identify a footer
SL_STATUS_INVALID_SIGNATURE: In case of corrupted app footer metadata
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_get_app_footer
sl_status_t sl_btmesh_blob_storage_get_app_footer (sl_bt_uuid_64_t const * blob_id, uint16_t app_id, void * buffer, uint16_t * length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
| uint16_t | [in] | app_id | Identifier of the application data |
| void * | [out] | buffer | Pointer to footer buffer |
| uint16_t * | [inout] | length | Length of the buffer; contains the length of the data read in case of success |
Extracts footer information assigned to a given BLOB, belonging to an application identifier.
Returns
Status code
Return values
SL_STATUS_OK: In case of successful reading
SL_STATUS_NOT_FOUND: If app_id and blob_id don't identify a footer
SL_STATUS_INVALID_SIGNATURE: In case of corrupted app footer metadata
SL_STATUS_INVALID_PARAMETER: If buffer is too short
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_set_managed#
sl_status_t sl_btmesh_blob_storage_set_managed (sl_bt_uuid_64_t const * blob_id, uint16_t owner_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
| uint16_t | [in] | owner_id | Identifier of owner which the BLOB belongs to |
Set BLOB to be managed, meaning it won't be deleted.
Each managed BLOB is managed by a specific owner which is stored with BLOB. Unmanaged BLOBs will be deleted when out of available space.
Returns
Status code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_FLASH_PROGRAM_FAILED: In case write failed
SL_STATUS_FULL: If there is no free space to store owner_id
SL_STATUS_NOT_FOUND: If blob_id doesn't identify any footer
SL_STATUS_INVALID_SIGNATURE: If any footer is corrupted during search for empty space to write new app footer
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_is_managed#
bool sl_btmesh_blob_storage_is_managed (sl_bt_uuid_64_t const * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
Check if BLOB is managed.
See Also
Returns
Boolean value
Return values
true: BLOB is managed
false: BLOB isn't managed or BLOB does not exist
sl_btmesh_blob_storage_is_managed_by_owner#
bool sl_btmesh_blob_storage_is_managed_by_owner (sl_bt_uuid_64_t const * blob_id, uint16_t owner_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const * | [in] | blob_id | Identifier of the BLOB |
| uint16_t | [in] | owner_id | Identifier of expected owner |
Check if BLOB is managed by a specific owner.
See Also
Returns
Boolean value
Return values
true: BLOB belongs to the specified owner
false: BLOB belongs to another owner or BLOB is not managed or BLOB does not exist
sl_btmesh_blob_storage_get_managed_flag_size#
uint32_t sl_btmesh_blob_storage_get_managed_flag_size (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Return the size of managed flag on BLOB storage medium.
BLOB storage needs to distinguish managed and unmanaged BLOBs so it marks managed BLOBs as such which requires some space on the medium.
Returns
Size of managed flag on BLOB storage medium
sl_btmesh_blob_storage_get_blob_id_by_owner#
sl_status_t sl_btmesh_blob_storage_get_blob_id_by_owner (uint16_t owner_id, uint32_t occurrence_idx, sl_bt_uuid_64_t * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | owner_id | Identifier of owner which the BLOB belongs to |
| uint32_t | [in] | occurrence_idx | Selects a BLOB from BLOBs managed by the same owner. Zero means the first BLOB with matching owner found during the search. |
| sl_bt_uuid_64_t * | [out] | blob_id | Identifier of the BLOB |
Searches BLOBs managed by a specific owner and provides the BLOB ID of the requested occurrence.
The search order for managed BLOBs of an owner is not specified but it is guaranteed that the order does not change unless new BLOB is added or an existing BLOB of the same owner is removed (delete, invalidate) from the BLOB storage.
When a managed BLOB belonging to an owner is removed from BLOB storage then occurrence_idx of BLOBs with same owner is decremented if the occurrence_idx of the BLOB was greater than the occurrence_idx of the removed BLOB otherwise the occurrence_idx does not change. In other words the BLOBs are shifted to lower indexes.
If a new managed BLOB is added by an owner to the BLOB storage then the search order of BLOBs with the same owner may change arbitrarily because it is not guaranteed which occurrence_idx the added BLOB is assigned to.
See Also
Returns
Result of managed BLOB ID get operation
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: If no BLOBs are found with owner_id or the occurrence_idx is greater or equal to the number of BLOBs managed by owner
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_get_blob_id_by_footer
sl_status_t sl_btmesh_blob_storage_get_blob_id_by_footer (uint16_t app_id, const void * expected_footer, uint16_t length, sl_bt_uuid_64_t * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | app_id | Identifier of the application data |
| const void * | [in] | expected_footer | Expected footer data for comparison |
| uint16_t | [in] | length | Length of the data |
| sl_bt_uuid_64_t * | [out] | blob_id | Identifier of the BLOB of the first match |
Searches for a specific app_id and data in the footer of each valid BLOB and returns the BLOB ID of the first match
Returns
Result of footer based BLOB ID query (propagates other internal errors)
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NOT_FOUND: If app_id is not found or the data is different
SL_STATUS_FAIL: In case of internal API error
sl_btmesh_blob_storage_get_total_space#
uint32_t sl_btmesh_blob_storage_get_total_space (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Queries total space for BLOB data storage in bytes (used + empty)
Returns
Total space in bytes
sl_btmesh_blob_storage_get_remaining_space#
uint32_t sl_btmesh_blob_storage_get_remaining_space (bool include_unmanaged_blobs)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | include_unmanaged_blobs | If true then unmanaged blobs are calculated into the remaining empty space. |
Queries remaining empty bytes in the BLOB storage
Returns
Remaining empty bytes
sl_btmesh_blob_storage_get_max_blob_size#
uint32_t sl_btmesh_blob_storage_get_max_blob_size (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Queries maximum BLOB size which can be stored if the whole BLOB storage is empty
Note
This might not be available even if one BLOB is stored
Returns
Maximum BLOB size
sl_btmesh_blob_storage_get_max_blob_size_free#
uint32_t sl_btmesh_blob_storage_get_max_blob_size_free (bool include_unmanaged_blobs)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | include_unmanaged_blobs | If true then unmanaged blobs are calculated into the maximum free BLOB size. |
Queries maximum BLOB size which can be stored in the free space of BLOB storage
Returns
Maximum supported BLOB size in free part of the BLOB storage
sl_btmesh_blob_storage_get_max_blob_count#
uint32_t sl_btmesh_blob_storage_get_max_blob_count (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Queries maximum number of BLOBs which can be stored
Returns
Maximum number of BLOBs
sl_btmesh_blob_storage_get_alignment#
uint8_t sl_btmesh_blob_storage_get_alignment (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Queries the BLOB storage alignment
Writes to the BLOB storage must have an offset that is aligned to this value. Apart from the last write of a writing procedure, the length of the data must be a multiple of this value. The last write can be of any length.
Returns
The BLOB storage alignment
sl_btmesh_blob_storage_get_erase_error_code#
sl_btmesh_blob_storage_delete_state_t sl_btmesh_blob_storage_get_erase_error_code (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Queries the error code/state of the asynchronous erase
Returns
State of asynchronous erase
Return values
SL_BTMESH_BLOB_STORAGE_DELETE_INACTIVE: If erase is inactive
SL_BTMESH_BLOB_STORAGE_DELETE_BUSY: If erase is ongoing
SL_BTMESH_BLOB_STORAGE_DELETE_FAILED: If erase has failed
SL_BTMESH_BLOB_STORAGE_DELETE_SUCCESS: If erase is successful
sl_btmesh_blob_storage_delete_step_handle#
void sl_btmesh_blob_storage_delete_step_handle (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Handles the asynchronous erase state machine
sl_btmesh_blob_storage_is_ok_to_sleep#
bool sl_btmesh_blob_storage_is_ok_to_sleep ()
Check if BLOB Storage allows the system to sleep
Returns
If it is ok to sleep
Return values
true: The system is allowed to sleep
false: The system shall be kept awake
Asynchronous erase requires the device to stay awake to finish.
sl_btmesh_blob_storage_calculate_checksum#
uint32_t sl_btmesh_blob_storage_calculate_checksum (const uint8_t * data, uint16_t length, uint32_t initial_value)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | data | Pointer to the app footer data |
| uint16_t | [in] | length | Length of the app footer length |
| uint32_t | [in] | initial_value | Initial value for checksum calculation |
Called when app footer is written to BLOB storage to calculate the checksum over app footer data
This is a callback which can be implemented in the application. Note
If no implementation is provided in the application, then the default weak implementation calculates Berger code.
Returns
Checksum calculated from app footer data