Btmesh Custom Role#
This component makes it possible to initialize a mesh device as a provisionee or provisioner based on application logic. For example an application could be implemented in a way that the device becomes a provisioner permanently when button is pressed at power up, otherwise it is just a provisionee. The sl_btmesh_custom_role_init weak callback function is called on boot event and the application is able to override this function to call one of the following initializer BT Mesh stack APIs: - sl_btmesh_node_init - sl_btmesh_node_init_oob - sl_btmesh_prov_init This component is prepared for integration into SOC applications.
Function Documentation#
sl_bt_custom_role_on_event#
void sl_bt_custom_role_on_event (sl_bt_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Pointer to incoming event. |
Handle BLE events for the mesh custom role.
This function is called automatically after enabling the component.
sl_btmesh_custom_role_init#
void sl_btmesh_custom_role_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Called on boot event and the application is able to override this function to initialize the device as a provisioner or as a provisionee.
The application should call one of the following BT Mesh stack initializer APIs based on implementation-specific logic:
sl_btmesh_node_init
sl_btmesh_node_init_oob
sl_btmesh_prov_init
This is a callback (weak function) which can be implemented in the application. Note
If no implementation is provided in the application, then the default weak implementation will be an empty function, and the application shall handle the sl_bt_evt_system_boot_id event by calling the mentioned APIs.