Firmware Distribution Server#
Provides BT Mesh Firmware Distribution Server functionality, defined in mesh specification. This model is used by the Distributor to receive from the Initiator the firmware update parameters, the set of Target nodes to update, and the firmware image to transfer. This model uses the Firmware Update Client model and the BLOB Transfer Client model to manage the firmware update. The Firmware Distribution Server can transfer one firmware image at a time. This component is prepared for integration into SOC applications. This is a No-Code component.
Functions#
Function Documentation#
sl_btmesh_fw_distribution_server_set_multicast_threshold#
sl_status_t sl_btmesh_fw_distribution_server_set_multicast_threshold (uint16_t elem_index, uint16_t multicast_threshold)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution Server model element index |
| uint16_t | [in] | multicast_threshold | If the number of servers for any step exceeds or is equal to this number then the group address will be used, otherwise servers will be looped through one by one. Value of 0 disables the feature. |
Set the multicast threshold value
The FW Distribution Server BT Mesh stack model caches the value of multicast threshold when the distribution is started and it passes the value to the MBT Client model (BLOB Transfer Client) in BT Mesh stack when the BLOB transfer is started. If the number of servers for any step exceeds or equal to this number then the group address will be used, otherwise the servers will be looped through one by one. Value of 0 disables the feature.
The MBT Client BT Mesh stack model tracks the number of servers which it needs to send specific messages to. It tracks for each server if the proper status message is received from the server in case of BLOB Information Get, BLOB Transfer Start, BLOB Block Start and BLOB Block Get messages. If some servers don't receive these BLOB messages or the response status messages are lost due to interference then the retry logic in BLOB Transfer Client SDK component requests to send the necessary BLOB messages to the servers by calling the proper MBT Client API again. If number of servers with missing status messages exceeds or equal to the multicast threshold value then the mentioned messages are sent to the group address, otherwise servers will be looped through one by one.
The tracking of successful reception of Chunk Transfer Messages are different because these are tracked by block status procedure in case of push transfer mode or by partial block report procedure in case of pull transfer mode.
The advantage of multicast messages is that the client needs to send one message only to the servers which is much faster if the number of servers which haven't received the message is high. This is especially true for chunk transfer because Chunk Transfer messages can be quite big and there are quite many of them in the BLOB Transfer.
The advantage of unicast addressing in case of non-chunk messages is that only those server respond with status messages which really need to. This can have significant effect when the node count is high. For example if there are hundreds of nodes in the BLOB transfer then each group message triggers hundreds of status messages even when only some status messages from specific servers are missing on the client side. The transport layer uses segment acknowledgment for segmented unicast mesh messages which improves the reliability of segmented message transfer especially when the number of segments are high but it tends to be slower because the segment acknowledgment messages needs to be waited.
Warnings
The MBT client stack model allocates and sends all unicast BLOB messages to each server at the same time below the multicast threshold. This could lead to exhaustive buffer allocation and the maximum number of parallel segmented messages can be exceeded as well in case of high multicast threshold level. The multicast threshold shall not be greater than SL_BTMESH_CONFIG_MAX_SEND_SEGS from sl_btmesh_config.h.
Note
The multicast threshold shall be set when the distribution is started (or before) in order to have an effect on the BLOB transfer otherwise it affects the next transfer only. The multicast threshold can be set in sl_btmesh_fw_distribution_server_on_distribution_started callback as well to tune it to the specific FW distribution.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_fw_distribution_server_on_event#
void sl_btmesh_fw_distribution_server_on_event (const sl_btmesh_msg_t *const evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_btmesh_msg_t *const | [in] | evt | Pointer to incoming event. |
Handle Firmware Distribution Server events
This function is called automatically after enabling the component.
sl_btmesh_fw_distribution_server_distribution_state_to_string#
const char * sl_btmesh_fw_distribution_server_distribution_state_to_string (sl_btmesh_fw_dist_server_dist_step_t state)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_fw_dist_server_dist_step_t | [in] | state | Distribution state |
Provides string representations of Distribution states
Returns
String representation of distribution state
Return values
INVALID: if the state is invalid
sl_btmesh_fw_distribution_server_node_phase_to_string#
const char * sl_btmesh_fw_distribution_server_node_phase_to_string (sl_btmesh_fw_dist_server_dist_node_phase_t node_phase)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_fw_dist_server_dist_node_phase_t | [in] | node_phase | Phase of Firmware Update Server on Target Node |
Provides string representations of Firmware Update phase
Returns
String representation of node update phase
Return values
INVALID: if the node_phase is invalid
sl_btmesh_fw_distribution_server_firmware_update_status_to_string#
const char * sl_btmesh_fw_distribution_server_firmware_update_status_to_string (sl_btmesh_fw_update_server_update_status_t node_status)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_fw_update_server_update_status_t | [in] | node_status | Status of Firmware Update Server on Target Node |
Provides string representations of Firmware Update status
Returns
String representation of node's firmware update status
Return values
INVALID: if the node_status is invalid
sl_btmesh_fw_distribution_server_generate_blob_id#
sl_status_t sl_btmesh_fw_distribution_server_generate_blob_id (sl_bt_uuid_64_t * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t * | [out] | blob_id | Pointer to blob_id where the generated bytes shall be stored |
Called to generate BLOB ID for firmware distribution
This is a callback which can be implemented in the application Note
If no implementation is provided in the application then a default weak implementation is provided which uses the sl_bt_system_get_random_data BT stack API to generate random bytes for BLOB identifier.
Returns
Status of BLOB id generation. If it is not SL_STATUS_OK then the firmware distribution server component uses the storage BLOB id for the firmware distribution. The storage BLOB id was used during firmware upload.
sl_btmesh_fw_distribution_server_on_node_added#
void sl_btmesh_fw_distribution_server_on_node_added (uint16_t elem_index, uint16_t server_address, uint8_t update_fw_image_idx, uint16_t node_count)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | server_address | Unicast address of the added target node |
| uint8_t | [in] | update_fw_image_idx | Firmware image index on target node to be updated during the distribution |
| uint16_t | [in] | node_count | Total number of target nodes which participates in the firmware distribution (including this new one) |
Called when a receiver target node is added to the firmware distribution list
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_all_nodes_deleted#
void sl_btmesh_fw_distribution_server_on_all_nodes_deleted (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
Called when all receiver target nodes are deleted from the firmware distribution list
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_distribution_started#
void sl_btmesh_fw_distribution_server_on_distribution_started (uint16_t elem_index, uint16_t client_address, uint16_t group_address, uint8_t ttl, sl_btmesh_fw_dist_server_dfu_policy_t update_policy, uint16_t fw_list_index, uint16_t timeout_base, sl_btmesh_mbt_client_transfer_mode_t transfer_mode, uint16_t node_count)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client |
| uint16_t | [in] | group_address | Group address of the distribution |
| uint8_t | [in] | ttl | Distribution TTL |
| sl_btmesh_fw_dist_server_dfu_policy_t | [in] | update_policy | 1 if the Update Policy is Verify and Apply, otherwise 0 |
| uint16_t | [in] | fw_list_index | Index of the firmware in the Distributor's FW List |
| uint16_t | [in] | timeout_base | Timeout base |
| sl_btmesh_mbt_client_transfer_mode_t | [in] | transfer_mode | Transfer Mode to use in the distribution |
| uint16_t | [in] | node_count | Total number of target nodes which participates in the firmware distribution |
Called when firmware distribution is started
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
The sl_btmesh_fw_distribution_server_set_multicast_threshold function can be called from this callback to set the multicast threshold value for the current distribution.
sl_btmesh_fw_distribution_server_on_distribution_canceled#
void sl_btmesh_fw_distribution_server_on_distribution_canceled (uint16_t elem_index, uint16_t client_address)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client |
Called when firmware distribution is canceled
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_distribution_suspended#
void sl_btmesh_fw_distribution_server_on_distribution_suspended (uint16_t elem_index, uint16_t client_address)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client |
Called when firmware distribution is suspended
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_distribution_resumed#
void sl_btmesh_fw_distribution_server_on_distribution_resumed (uint16_t elem_index, uint16_t client_address, uint16_t group_address, uint8_t ttl, sl_btmesh_fw_dist_server_dfu_policy_t update_policy, uint16_t fw_list_index, uint16_t timeout_base, sl_btmesh_mbt_client_transfer_mode_t transfer_mode, uint16_t node_count)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client |
| uint16_t | [in] | group_address | Group address of the distribution |
| uint8_t | [in] | ttl | Distribution TTL |
| sl_btmesh_fw_dist_server_dfu_policy_t | [in] | update_policy | 1 if the Update Policy is Verify and Apply, otherwise 0 |
| uint16_t | [in] | fw_list_index | Index of the firmware in the Distributor's FW List |
| uint16_t | [in] | timeout_base | Timeout base |
| sl_btmesh_mbt_client_transfer_mode_t | [in] | transfer_mode | Transfer Mode to use in the distribution |
| uint16_t | [in] | node_count | Total number of target nodes which participates in the firmware distribution |
Called when firmware distribution is suspended
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_distribution_state_changed#
void sl_btmesh_fw_distribution_server_on_distribution_state_changed (uint16_t elem_index, sl_btmesh_fw_dist_server_dist_step_t state, uint16_t num_active_nodes, uint16_t node_count)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| sl_btmesh_fw_dist_server_dist_step_t | [in] | state | Distribution state |
| uint16_t | [in] | num_active_nodes | Number of target nodes which are still active |
| uint16_t | [in] | node_count | Total number of target nodes |
Called when firmware distribution state has changed
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_distribution_blob_progress_changed#
void sl_btmesh_fw_distribution_server_on_distribution_blob_progress_changed (uint16_t elem_index, uint32_t confirmed_tx_bytes, uint32_t blob_size, uint16_t node_count)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint32_t | [in] | confirmed_tx_bytes | Number of BLOB bytes which are received by every active BLOB Transfer Server. The progress is calculated at the end of the blocks because in a block some chunks could be retransmitted multiple times. |
| uint32_t | [in] | blob_size | Size of the BLOB |
| uint16_t | [in] | node_count | Number of target nodes |
Called when progress of BLOB transfer step during the firmware distribution has changed
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_distribution_node_failed#
void sl_btmesh_fw_distribution_server_on_distribution_node_failed (uint16_t elem_index, uint16_t server_address, sl_btmesh_fw_dist_server_dist_node_phase_t update_phase, sl_btmesh_fw_update_server_update_status_t update_status, uint8_t mbt_status, uint8_t progress, uint8_t fw_index, uint16_t num_active_nodes, uint16_t node_count)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | server_address | Unicast address of the failed Target Node |
| sl_btmesh_fw_dist_server_dist_node_phase_t | [in] | update_phase | Update Phase of Firmware Update Server on Target Node |
| sl_btmesh_fw_update_server_update_status_t | [in] | update_status | Update Status of Firmware Update Server on Target Node If the firmware update of the node fails due to Firmware Update Server related error then this field isn't zero and it has sl_btmesh_fw_update_server_update_status_t value. |
| uint8_t | [in] | mbt_status | Transfer status of BLOB Transfer server on Target Node. If the firmware update of a node fails due to BLOB Transfer error then this field won't be zero. |
| uint8_t | [in] | progress | 0-100, percentage of BLOB Transfer octets |
| uint8_t | [in] | fw_index | Firmware image index on Target node which is updated during the distribution |
| uint16_t | [in] | num_active_nodes | Number of target nodes which are still active |
| uint16_t | [in] | node_count | Total number of target nodes |
Called when a Target Node fails during the distribution
If one node fails during the distribution, it does not mean, that the distribution fails as well. The distribution only fails, when every Target Node fails.
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_firmware_added#
void sl_btmesh_fw_distribution_server_on_firmware_added (uint16_t elem_index, uint16_t client_address, uint32_t fw_size, uint16_t fw_list_idx, uint16_t current_fw_list_length, uint16_t max_fw_list_length, const uint8_t * fwid, uint8_t fwid_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client Set to unassigned address (0x0000) when the firmware is added at init time. |
| uint32_t | [in] | fw_size | Size of the firmware binary image |
| uint16_t | [in] | fw_list_idx | Index of the stored firmware in the firmware list |
| uint16_t | [in] | current_fw_list_length | Current number of stored firmware including this uploaded firmware as well. |
| uint16_t | [in] | max_fw_list_length | Maximum number of firmwares which can be stored on the Distributor |
| const uint8_t * | [in] | fwid | Firmware identifier with 2-byte Company ID which is followed by 0-106 bytes of Version Information |
| uint8_t | [in] | fwid_length | Length of the Firmware identifier data |
Called when firmware has been added to the Distributor
Called when a new firmware has been uploaded to the Distributor
Called when the firmware has been added based on the NVM content at initialization time
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_firmware_deleted#
void sl_btmesh_fw_distribution_server_on_firmware_deleted (uint16_t elem_index, uint16_t client_address, uint16_t current_fw_list_length, uint16_t max_fw_list_length, const uint8_t * fwid, uint8_t fwid_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client |
| uint16_t | [in] | current_fw_list_length | Current number of stored firmwares after the firmware is deleted from the Distributor |
| uint16_t | [in] | max_fw_list_length | Maximum number of firmwares which can be stored on the Distributor |
| const uint8_t * | [in] | fwid | Firmware identifier with 2-byte Company ID which is followed by 0-106 bytes of Version Information |
| uint8_t | [in] | fwid_length | Length of the Firmware identifier data |
Called when a firmware has been deleted from the Distributor
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_on_all_firmware_deleted#
void sl_btmesh_fw_distribution_server_on_all_firmware_deleted (uint16_t elem_index, uint16_t client_address, uint16_t max_fw_list_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Distribution server model element index |
| uint16_t | [in] | client_address | Address of the Distribution Client It is set to MESH_ADDR_UNASSIGNED when it is caused by an internal event. |
| uint16_t | [in] | max_fw_list_length | Maximum number of firmwares which can be stored on the Distributor |
Called when ALL firmwares are deleted from the Distributor
This is a callback which can be implemented in the application Note
If no implementation is provided in the application, then the default weak implementation will be an empty function.
sl_btmesh_fw_distribution_server_delete_step_handle#
void sl_btmesh_fw_distribution_server_delete_step_handle (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Used for asynchronously deleting firmware images from BLOB storage