BT Mesh Remote Provisioner Application Component#
BT Mesh Remote Provisioner Application component provides application-level functionality for remote provisioning of devices in Bluetooth Mesh networks.
Functions#
Macros#
Optstring argument for getopt.
Optstring argument for getopt.
Usage info.
Function Documentation#
btmesh_app_remote_prov_init#
sl_status_t btmesh_app_remote_prov_init (int cmd_opt, char * cmd_optarg)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | [in] | cmd_opt | Command option |
| char * | [in] | cmd_optarg | Command argument |
Remote Provisioner Command Line Application Init
btmesh_app_remote_prov_process_action#
void btmesh_app_remote_prov_process_action (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Remote Provisioner Application Process Action
btmesh_app_remote_prov_on_event#
void btmesh_app_remote_prov_on_event (sl_btmesh_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_msg_t * | [in] | evt | Event coming from the Bluetooth Mesh stack |
Bluetooth Mesh stack event handler
btmesh_app_remote_prov_get_command#
void btmesh_app_remote_prov_get_command (command_t * remote_prov_command, command_state_t * remote_prov_command_state)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| command_t * | [out] | remote_prov_command | Current command |
| command_state_t * | [out] | remote_prov_command_state | Current command status |
Get the remote provisioner command and command status
btmesh_app_remote_prov_set_command#
void btmesh_app_remote_prov_set_command (command_t remote_prov_command)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| command_t | [in] | remote_prov_command | New command |
Set the remote provisioner command
btmesh_app_remote_prov_set_command_state#
void btmesh_app_remote_prov_set_command_state (command_state_t remote_prov_command_state)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| command_state_t | [out] | remote_prov_command_state | New command status |
Set the remote provisioner command status
btmesh_app_remote_prov_end_of_cmd#
void btmesh_app_remote_prov_end_of_cmd (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Callback to inform when the command ends
btmesh_app_remote_prov_get_server_address#
bool btmesh_app_remote_prov_get_server_address (uint16_t * ui_server_address)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [out] | ui_server_address | The variable to fill with server address |
Get remote provisioning server address from UI
btmesh_app_remote_prov_get_prov_data#
bool btmesh_app_remote_prov_get_prov_data (uint16_t * remote_prov_server_addr, uuid_128 * remote_prov_uuid, uint16_t * remote_prov_oob_capabilities)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [out] | remote_prov_server_addr | The variable to fill with server address |
| uuid_128 * | [out] | remote_prov_uuid | The variable to fill with unprovisioned node uuid |
| uint16_t * | [out] | remote_prov_oob_capabilities | The variable to fill with unprovisioned node OOB capability bitmask |
Get remote provisioning server address and unprovisioned node uuid from UI
Macro Definition Documentation#
REMOTE_PROV_USAGE#
#define REMOTE_PROV_USAGEValue:
Usage info.
REMOTE_PROV_OPTIONS#
#define REMOTE_PROV_OPTIONSValue:
LONG_OPT_SIZE#
#define LONG_OPT_SIZEValue:
PROV_OPTLENGTH + REMOTE_PROV_OPTLENGTH + CBP_OPTLENGTH + LAST_OPTION_ELEMENT
OPTSTRING#
#define OPTSTRINGValue:
NCP_HOST_OPTSTRING PROV_OPTSTRINGREMOTE_PROV_OPTSTRING CBP_OPTSTRING "h"
OPTIONS#
#define OPTIONSValue: