Sensor Server#
Used to support the reporting functionality of a node with a set of sensors whose data is available on the network. It also has a corresponding Sensor Setup Server model which is present on the same element. This component implements temperature, people count, and illuminance measurements. It provides callback functions for each property. This component is prepared for integration into SOC applications. This is a No-Code component if using a Silicon Labs device and the relevant components for their respective hardware.
Functions#
Macros#
Represents an unknown value for power consumption sensor data.
Represents an invalid value for power consumption sensor data.
Represents an unknown light measurement value for the light sensor.
Represents an unknown temperature value for the temperature sensor.
Function Documentation#
sl_btmesh_sensor_server_node_init#
void sl_btmesh_sensor_server_node_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize Sensor Server.
This function is called automatically after enabling the component.
sl_btmesh_handle_sensor_server_events#
void sl_btmesh_handle_sensor_server_events (sl_btmesh_msg_t * pEvt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_msg_t * | [in] | pEvt | Sensor server event to handle |
Handle Sensor Server events.
This function is called automatically after enabling the component.
sl_btmesh_sensor_server_on_temperature_measurement#
void sl_btmesh_sensor_server_on_temperature_measurement (temperature_8_t temperature)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| temperature_8_t | [in] | temperature | Temperature value in 0.5 degree Celsius steps |
Called when a temperature measurement is done Note
If no implementation is provided in the application then a default weak implementation if provided which is a no-operation. (empty function)
sl_btmesh_sensor_server_on_light_measurement#
void sl_btmesh_sensor_server_on_light_measurement (illuminance_t light)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| illuminance_t | [in] | light | Lightness value in lux |
Called when a light measurement is done Note
If no implementation is provided in the application then a default weak implementation if provided which is a no-operation. (empty function)
sl_btmesh_sensor_server_on_people_count_measurement#
void sl_btmesh_sensor_server_on_people_count_measurement (count16_t people)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| count16_t | [in] | people | People count sensor value |
Called when a people count sensor measurement is done Note
If no implementation is provided in the application then a default weak implementation if provided which is a no-operation. (empty function)
sl_btmesh_sensor_server_on_energy_monitor_measurement#
void sl_btmesh_sensor_server_on_energy_monitor_measurement (energy32_t power_consumption)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| energy32_t | [in] | power_consumption | Power consumption measured by the energy monitor |
Called when an energy monitor measurement is done Note
If no implementation is provided in the application then a default weak implementation if provided which is a no-operation. (empty function)