Bluetooth Mesh Solicitation PDU RPL Config Client#
Provides a thin layer to automatically initialize the Solicitation PDU RPL Config Client model. The model then can be used to remove addresses from the solicitation replay protection list of a node that supports the Solicitation PDU RPL Configuration Server model. This is a No-Code component.
Functions#
void
sl_btmesh_solicitation_config_client_on_event(const sl_btmesh_msg_t *const evt)
Function Documentation#
sl_btmesh_solicitation_config_client_on_event#
void sl_btmesh_solicitation_config_client_on_event (const sl_btmesh_msg_t *const evt)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_btmesh_msg_t *const | [in] | evt | Pointer to incoming event. |
Handle Solicitation Config Client events.
This function is called automatically after enabling the component.