NCP Advertisement Extension Client#
NCP Advertisement Extension Client component enables the Silabs Configuration Client vendor model for the node. Silabs Configuration Client can setup other nodes with Silabs Configuration Server Feature enabled (e.g. by the Advertisement Extension Server component). This is a proprietary feature which breaks compliance with AE in BT Mesh 1.1 specification. This component is prepared for integration into NCP applications. This is a No-Code component.