Install and Configure Packages#
Follow these steps to install and set up the Command Line Development environment.
Download SLT from the Command Line Development page.
Create the recipe file,
cli_tool.toml, per the instructions in Packages to Install with SLT.Edit the
pathsystem variable to add thesltpath.In Windows, type Edit System Variables in the search field to find the System Properties pop-up.
Select Environment Variables.
Edit the 'Path' variable.
Click Browse to add the slt executable from the expanded zip file that was downloaded in step 1.
Open a terminal or command prompt.
Change the directory by typing
cdto theusers\USERNAMEfolder and enter the command,slt install –f cli_tools.toml.Add the paths to Java and
slc_clito thepathsystem variable. The paths are your .silabs folder. The names might be slightly different, depending on the version of the package you have..silabs\slt\installs\archive\java21-v21.0.5\java21_windows_x86_64\jre\bin.silabs\slt\installs\archive\slc_cli_base-v6.0.9\slc_cli
Configure SLC for the toolchain and SDK to be used. The SDK also needs to be trusted for SLC to use the SDK in project operations:
slc configuration –s .silabs\slt\installs\conan\p\simpldxxxxx\pslc signature trustslc configuration –gcc .silabs\slt\installs\conan\p\gcc-xxxxx\p