Sample API functions for using push-buttons. More...
Functions |
|
| void | halInternalInitButton (void) |
|
Initializes the buttons. This function is automatically called by
halInit()
.
More...
|
|
| uint8_t | halButtonState (uint8_t button) |
|
Returns the current state (pressed or released) of a button.
More...
|
|
| uint8_t | halButtonPinState (uint8_t button) |
|
Returns the current state (pressed or released) of the pin associated with a button.
More...
|
|
| void | halButtonIsr (uint8_t button, uint8_t state) |
|
A callback called in interrupt context whenever a button changes its state.
More...
|
|
Button State Definitions |
|
|
A set of numerical definitions for use with the button APIs indicating the state of a button. |
|
| #define | BUTTON_PRESSED 1 |
|
Button state is pressed.
More...
|
|
| #define | BUTTON_RELEASED 0 |
|
Button state is released.
More...
|
|
Detailed Description
Sample API functions for using push-buttons.
See
button.h
for source code.
Macro Definition Documentation
| #define BUTTON_PRESSED 1 |
Button state is pressed.
Definition at line
24
of file
button.h
.
| #define BUTTON_RELEASED 0 |
Button state is released.
Definition at line
28
of file
button.h
.
Function Documentation
| void halButtonIsr | ( | uint8_t |
button,
|
| uint8_t |
state
|
||
| ) |
A callback called in interrupt context whenever a button changes its state.
- Application Usage:
- Must be implemented by the application. This function should contain the functionality to be executed in response to changes of state in each of the buttons, or callbacks to the appropriate functionality.
- Parameters
-
buttonThe button which has changed state, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER. stateThe new state of the button referenced by the button parameter, either BUTTON_PRESSED if the button has been pressed or BUTTON_RELEASED if the button has been released.
| uint8_t halButtonPinState | ( | uint8_t |
button
|
) |
Returns the current state (pressed or released) of the pin associated with a button.
This reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.
- Parameters
-
buttonThe button being queried, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER.
- Returns
- BUTTON_PRESSED if the button is pressed or BUTTON_RELEASED if the button is not pressed.
| uint8_t halButtonState | ( | uint8_t |
button
|
) |
Returns the current state (pressed or released) of a button.
- Note
- This function is correlated with halButtonIsr() and so returns the shadow state rather than reading the actual state of the pin.
- Parameters
-
buttonThe button being queried, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER.
- Returns
- BUTTON_PRESSED if the button is pressed or BUTTON_RELEASED if the button is not pressed.
| void halInternalInitButton | ( | void |
|
) |
Initializes the buttons. This function is automatically called by halInit() .