|
|
|
uint16_t
|
NTOHS
(uint16_t val)
|
|
|
Converts a short (16-bit) value from network to host byte order.
More...
|
|
|
|
uint32_t
|
NTOHL
(uint32_t val)
|
|
|
Converts a long (32-bit) value from network to host byte order.
More...
|
|
|
|
uint32_t
|
SwapEndiannessInt32u
(uint32_t val)
|
|
|
*/
Functions that provide conversions from network to host byte order. Network byte order is big endian, so these APIs are only necessary on platforms which have a natural little endian byte order. On big-endian platforms, the APIs are macro'd away to nothing. See
endian.h
for source code.
Definition at line
61
of file
endian.h
.
Definition at line
64
of file
endian.h
.
|
uint32_t NTOHL
|
(
|
uint32_t
|
val
|
)
|
|
Converts a long (32-bit) value from network to host byte order.
|
uint16_t NTOHS
|
(
|
uint16_t
|
val
|
)
|
|
Converts a short (16-bit) value from network to host byte order.
|
uint32_t SwapEndiannessInt32u
|
(
|
uint32_t
|
val
|
)
|
|