EmberNetworkParameters Struct Reference
Holds network parameters. More...
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | panId |
| int8_t | radioTxPower |
| uint8_t | radioChannel |
Holds network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit.
Definition at line
151
of file
ember-types.h
.
Field Documentation
| uint16_t EmberNetworkParameters::panId |
The network's PAN identifier.
Definition at line
153
of file
ember-types.h
.
| uint8_t EmberNetworkParameters::radioChannel |
A radio channel. Be sure to specify a channel supported by the radio.
Definition at line
157
of file
ember-types.h
.
| int8_t EmberNetworkParameters::radioTxPower |
A power setting, in dBm.
Definition at line
155
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h