EmberOutgoingMessage Struct Reference
An instance of this structure is passed to emberMessageSentHandler() . It describes the outgoing packet. More...
#include <
ember-types.h
>
Data Fields |
|
| EmberMessageOptions | options |
| EmberNodeId | destination |
| uint8_t | endpoint |
| uint8_t | tag |
| EmberMessageLength | length |
| uint8_t * | payload |
| int8_t | ackRssi |
An instance of this structure is passed to emberMessageSentHandler() . It describes the outgoing packet.
Definition at line
262
of file
ember-types.h
.
Field Documentation
◆ ackRssi
| int8_t EmberOutgoingMessage::ackRssi |
The RSSI in dBm of the ACK corresponding to this message. This field is meaningful only if EMBER_OPTIONS_ACK_REQUESTED flag is set in the options field.
Definition at line
295
of file
ember-types.h
.
◆ destination
| EmberNodeId EmberOutgoingMessage::destination |
An EmberNodeId value indicating the destination short ID.
Definition at line
271
of file
ember-types.h
.
◆ endpoint
| uint8_t EmberOutgoingMessage::endpoint |
The endpoint the message is destined to.
Definition at line
275
of file
ember-types.h
.
◆ length
| EmberMessageLength EmberOutgoingMessage::length |
An EmberMessageLength value indicating the length in bytes of the incoming message.
Definition at line
285
of file
ember-types.h
.
◆ options
| EmberMessageOptions EmberOutgoingMessage::options |
An EmberMessageOptions value indicating the options used for transmitting the outgoing message.
Definition at line
267
of file
ember-types.h
.
◆ payload
| uint8_t* EmberOutgoingMessage::payload |
A pointer to the message payload.
Definition at line
289
of file
ember-types.h
.
◆ tag
| uint8_t EmberOutgoingMessage::tag |
A tag value the application can use to match emberMessageSend() calls to the corresponding emberMessageSentHandler() calls.
Definition at line
280
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h