tokTypeStackNodeData Struct Reference
Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token. More...
#include <
token-stack.h
>
Data Fields |
|
| uint16_t | panId |
| int8_t | radioTxPower |
| uint8_t | radioFreqChannel |
| uint8_t | nodeType |
| uint16_t | nodeId |
| uint16_t | parentId |
Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token.
The key itself
Definition at line
231
of file
token-stack.h
.
Field Documentation
◆ nodeId
| uint16_t tokTypeStackNodeData::nodeId |
The NodeId (short address) of the device
Definition at line
236
of file
token-stack.h
.
◆ nodeType
| uint8_t tokTypeStackNodeData::nodeType |
The EmberNodeType configured for the device
Definition at line
235
of file
token-stack.h
.
◆ panId
| uint16_t tokTypeStackNodeData::panId |
The PanId of the device
Definition at line
232
of file
token-stack.h
.
◆ parentId
| uint16_t tokTypeStackNodeData::parentId |
The NodeId of the device's parent, if any
Definition at line
237
of file
token-stack.h
.
◆ radioFreqChannel
| uint8_t tokTypeStackNodeData::radioFreqChannel |
The radio channel configured for the device
Definition at line
234
of file
token-stack.h
.
◆ radioTxPower
| int8_t tokTypeStackNodeData::radioTxPower |
The TX power configured for the device in dBm
Definition at line
233
of file
token-stack.h
.
The documentation for this struct was generated from the following file:
-
token-stack.h