Parent Support
Functions |
|
| EmberStatus | emberFormNetwork ( EmberNetworkParameters *parameters) |
|
Form a new network by becoming the coordinator. This API requires the parent-support library to be present.
More...
|
|
| EmberStatus | emberGetChildFlags ( EmberMacAddress *address, EmberChildFlags *flags) |
|
Return an
EmberChildFlags
bitmask indicating the child flags of the child corresponding to the passed MAC address.
More...
|
|
| EmberStatus | emberRemoveChild ( EmberMacAddress *address) |
|
Remove the node corresponding to the passed MAC address from the child table.
More...
|
|
| EmberStatus | emberPurgeIndirectMessages (void) |
|
Purge all indirect transmissions from the indirect message queue.
More...
|
|
| EmberStatus | emberSetIndirectQueueTimeout (uint32_t timeoutMs) |
|
Set indirect queue timeout value. The indirect queue timeout is set by default to
EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS
.
More...
|
|
Handlers |
|
| void | emberChildJoinHandler ( EmberNodeType nodeType, EmberNodeId nodeId) |
|
This handler is invoked at coordinator, range extender, or mac mode nodes when a new child has joined the device.
More...
|
|
Function Documentation
◆ emberChildJoinHandler()
| void emberChildJoinHandler | ( | EmberNodeType |
nodeType,
|
| EmberNodeId |
nodeId
|
||
| ) |
This handler is invoked at coordinator, range extender, or mac mode nodes when a new child has joined the device.
- Parameters
-
[in] nodeTypeThe role of the joining device ( EMBER_STAR_RANGE_EXTENDER , EMBER_STAR_END_DEVICE , EMBER_STAR_SLEEPY_END_DEVICE , EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE ). [in] nodeIdThe node ID of the joining device.
◆ emberFormNetwork()
| EmberStatus emberFormNetwork | ( | EmberNetworkParameters * |
parameters
|
) |
Form a new network by becoming the coordinator. This API requires the parent-support library to be present.
- Parameters
-
[in] parametersAn EmberNetworkParameters value that specifies the network parameters of the network to be formed.
- Returns
-
An
EmberStatusvalue that indicates either the successful formation of the new network or the reason that the network formation failed.
◆ emberGetChildFlags()
| EmberStatus emberGetChildFlags | ( | EmberMacAddress * |
address,
|
| EmberChildFlags * |
flags
|
||
| ) |
Return an EmberChildFlags bitmask indicating the child flags of the child corresponding to the passed MAC address.
- Parameters
-
[in] addressA pointer to an EmberMacAddress that specifies the MAC address of the child. [out] flagsA pointer to an EmberChildFlags containing the child flags of the child corresponding to the passed MAC address.
- Returns
-
An
EmberStatusvalue of EMBER_SUCCESS if the child was found in the child table, or anotherEmberStatusvalue indicating the reason of failure.
◆ emberPurgeIndirectMessages()
| EmberStatus emberPurgeIndirectMessages | ( | void |
|
) |
Purge all indirect transmissions from the indirect message queue.
- Returns
-
an
EmberStatusvalue of EMBER_SUCCESS if all indirect messages were purged, or anotherEmberStatusvalue indicating the reason of failure.
◆ emberRemoveChild()
| EmberStatus emberRemoveChild | ( | EmberMacAddress * |
address
|
) |
Remove the node corresponding to the passed MAC address from the child table.
- Parameters
-
[in] addressA pointer to an EmberMacAddress that specifies the MAC address of the child to be removed.
- Returns
-
An
EmberStatusvalue of EMBER_SUCCESS if the node was successfully removed from the child table, or anotherEmberStatusvalue indicating the reason of failure.
◆ emberSetIndirectQueueTimeout()
| EmberStatus emberSetIndirectQueueTimeout | ( | uint32_t |
timeoutMs
|
) |
Set indirect queue timeout value. The indirect queue timeout is set by default to EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS .
- Parameters
-
timeoutMsThe timeout in milliseconds to be set.
- Returns
-
an
EmberStatusvalue of EMBER_SUCCESS if the passed timeout was successfully set, or a value of EMBER_INVALID_CALL if the passed value is invalid.