EmberMacAddress Struct Reference
A structure that stores an 802.15.4 address. More...
#include <
ember-types.h
>
Data Fields |
|
| union { | |
| uint8_t longAddress [ EUI64_SIZE ] | |
Long (EUI-64) address. Valid if
mode
is
EMBER_MAC_ADDRESS_MODE_LONG
.
More...
|
|
| uint16_t shortAddress | |
Short address (node ID). Valid if
mode
is
EMBER_MAC_ADDRESS_MODE_SHORT
.
More...
|
|
| } | addr |
| EmberMacAddressMode | mode |
A structure that stores an 802.15.4 address.
Definition at line
332
of file
ember-types.h
.
Field Documentation
◆ addr
| union { ... } EmberMacAddress::addr |
◆ longAddress
| uint8_t EmberMacAddress::longAddress[ EUI64_SIZE ] |
Long (EUI-64) address. Valid if
mode
is
EMBER_MAC_ADDRESS_MODE_LONG
.
Definition at line
338
of file
ember-types.h
.
◆ mode
| EmberMacAddressMode EmberMacAddress::mode |
Addressing mode
Definition at line
346
of file
ember-types.h
.
◆ shortAddress
| uint16_t EmberMacAddress::shortAddress |
Short address (node ID). Valid if
mode
is
EMBER_MAC_ADDRESS_MODE_SHORT
.
Definition at line
343
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h