EmberNetworkParameters Struct Reference
Hold network parameters. More...
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | panId |
| int16_t | radioTxPower |
| uint16_t | radioChannel |
Hold network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit and the Radio Configurator Guide (AN971).
Definition at line
164
of file
ember-types.h
.
Field Documentation
◆ panId
| uint16_t EmberNetworkParameters::panId |
The network's PAN identifier.
Definition at line
166
of file
ember-types.h
.
◆ radioChannel
| uint16_t EmberNetworkParameters::radioChannel |
The radio channel. Be sure to specify a channel supported by the radio.
Definition at line
170
of file
ember-types.h
.
◆ radioTxPower
| int16_t EmberNetworkParameters::radioTxPower |
The transmit power setting, in deci-dBm.
Definition at line
168
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h