tokTypeStackChildTableEntry Struct Reference

Type of an element of TOKEN_STACK_CHILD_TABLE (indexed token). Keeps children information of a device, which has parent support enabled. More...

#include < token-stack.h >

Data Fields

EmberEUI64 longId
EmberNodeId shortId
uint8_t flags

Type of an element of TOKEN_STACK_CHILD_TABLE (indexed token). Keeps children information of a device, which has parent support enabled.

Definition at line 245 of file token-stack.h .

Field Documentation

◆ flags

uint8_t tokTypeStackChildTableEntry::flags

Flags for the child required by the stack

Definition at line 248 of file token-stack.h .

◆ longId

EmberEUI64 tokTypeStackChildTableEntry::longId

The Long Id of the child

Definition at line 246 of file token-stack.h .

◆ shortId

EmberNodeId tokTypeStackChildTableEntry::shortId

The NodeId of the child

Definition at line 247 of file token-stack.h .


The documentation for this struct was generated from the following file:
  • token-stack.h