Definitions of Connect data types used by various Connect API functions. More...

Data Structures

struct EmberNetworkParameters
Hold network parameters. More...
struct EmberIncomingMessage
An instance of this structure is passed to emberIncomingMessageHandler() . It describes the incoming message. More...
struct EmberOutgoingMessage
An instance of this structure is passed to emberMessageSentHandler() . It describes the outgoing packet. More...
struct EmberMacAddress
A structure that stores an 802.15.4 address. More...
struct EmberMacFrame
A structure that describes the addressing fields of a 802.15.4 frame. More...
struct EmberIncomingMacMessage
An instance of this structure is passed to emberIncomingMacMessageHandler() . It describes the incoming MAC frame. More...
struct EmberOutgoingMacMessage
An instance of this structure is passed to emberMacMessageSentHandler() . It describes the outgoing MAC frame. More...
struct EmberKeyData
This data structure contains the security key, most prominently used by emberSetSecurityKey . More...
struct EventActions
The static part of an event. Each event can be used with only one event queue. More...
struct Event_s
struct EventQueue_s
An event queue is currently just a list of events ordered by execution time. More...
struct EmberEventControl
Control structure for events. More...
struct EmberEventData_S
Complete events with a control and a handler procedure. More...
struct EmberTaskControl
Control structure for tasks. More...

Macros

#define EXTENDED_PAN_ID_SIZE 8
Size of an extended PAN identifier in bytes (8). More...
#define EUI64_SIZE 8
Size of EUI64 (an IEEE address) in bytes (8). More...
#define EMBER_ENCRYPTION_KEY_SIZE 16
Size of an encryption key in bytes (16). More...
#define EMBER_NULL_NODE_ID 0xFFFF
A distinguished network ID that will never be assigned to any node. Used to indicate the absence of a node ID. More...
#define EMBER_BROADCAST_ADDRESS 0xFFFF
Broadcast address. More...
#define EMBER_USE_LONG_ADDRESS 0xFFFE
Special short address indicating the node should use long addressing as source address. More...
#define EMBER_COORDINATOR_ADDRESS 0x0000
The coordinator short address. More...
#define EMBER_CAL_INVALID_VALUE (0xFFFFFFFF)

Typedefs

typedef uint8_t EmberEUI64 [ EUI64_SIZE ]
EUI 64-bit ID (IEEE 802.15.4 long address). More...
typedef uint16_t EmberNodeId
IEEE 802.15.4 node ID. Also known as short address. More...
typedef uint16_t EmberPanId
IEEE 802.15.4 PAN ID. More...
typedef uint8_t EmberMessageLength
Message length in bytes. More...
typedef uint8_t EmberTaskId
An identifier for a task. More...
typedef struct Event_s Event
typedef struct EventQueue_s EventQueue
An event queue is currently just a list of events ordered by execution time. More...
typedef PGM struct EmberEventData_S EmberEventData
typedef uint16_t EmberBuffer
Buffers used by the memory buffer system. More...

Enumerations

enum EmberNodeType {
EMBER_UNKNOWN_DEVICE = 0,
EMBER_STAR_COORDINATOR = 1,
EMBER_STAR_RANGE_EXTENDER = 2,
EMBER_STAR_END_DEVICE = 3,
EMBER_STAR_SLEEPY_END_DEVICE = 4,
EMBER_DIRECT_DEVICE = 5,
EMBER_MAC_MODE_DEVICE = 6,
EMBER_MAC_MODE_SLEEPY_DEVICE = 7
}
Define the possible types of nodes and the roles that a node might play in a network. More...
enum EmberNetworkStatus {
EMBER_NO_NETWORK ,
EMBER_JOINING_NETWORK ,
EMBER_JOINED_NETWORK ,
EMBER_RADIO_TEST
}
Defines the possible join states for a node. More...
enum EmberChildFlags {
EMBER_CHILD_FLAGS_DEVICE_IS_RANGE_EXTENDER_BIT = 0x02,
EMBER_CHILD_FLAGS_DEVICE_IS_SLEEPY_BIT = 0x04,
EMBER_CHILD_FLAGS_HAVE_PENDING_DATA_BIT = 0x08,
EMBER_CHILD_FLAGS_AES_SECURITY_CAPABLE_BIT = 0x10,
EMBER_CHILD_FLAG_DEVICE_IS_EXTENDED_BIT = 0x20
}
Child flags. More...
enum EmberMessageOptions {
EMBER_OPTIONS_NONE = 0x00,
EMBER_OPTIONS_SECURITY_ENABLED = 0x01,
EMBER_OPTIONS_ACK_REQUESTED = 0x02,
EMBER_OPTIONS_HIGH_PRIORITY = 0x04,
EMBER_OPTIONS_INDIRECT = 0x08
}
Message options. More...
enum EmberMacAddressMode {
EMBER_MAC_ADDRESS_MODE_NONE = 0x00,
EMBER_MAC_ADDRESS_MODE_SHORT = 0x02,
EMBER_MAC_ADDRESS_MODE_LONG = 0x03
}
802.15.4 addressing mode. More...
enum EmberEventUnits {
EMBER_EVENT_INACTIVE = 0,
EMBER_EVENT_MS_TIME ,
EMBER_EVENT_QS_TIME ,
EMBER_EVENT_MINUTE_TIME ,
EMBER_EVENT_ZERO_DELAY
}
Either marks an event as inactive or specifies the units for the event execution time. More...
enum {
EMBER_OUTGOING_MESSAGES = 0x0001,
EMBER_INCOMING_MESSAGES = 0x0002,
EMBER_RADIO_IS_ON = 0x0004,
EMBER_ASSOCIATING = 0x0008,
EMBER_SCANNING = 0x0010
}
Define tasks that prevent the stack from sleeping. More...
enum EmberCounterType {
EMBER_COUNTER_PHY_IN_PACKETS ,
EMBER_COUNTER_PHY_OUT_PACKETS ,
EMBER_COUNTER_MAC_IN_UNICAST ,
EMBER_COUNTER_MAC_IN_BROADCAST ,
EMBER_COUNTER_MAC_OUT_UNICAST_NO_ACK ,
EMBER_COUNTER_MAC_OUT_UNICAST_ACK_SUCCESS ,
EMBER_COUNTER_MAC_OUT_UNICAST_ACK_FAIL ,
EMBER_COUNTER_MAC_OUT_UNICAST_CCA_FAIL ,
EMBER_COUNTER_MAC_OUT_UNICAST_RETRY ,
EMBER_COUNTER_MAC_OUT_BROADCAST ,
EMBER_COUNTER_MAC_OUT_BROADCAST_CCA_FAIL ,
EMBER_COUNTER_MAC_OUT_ENCRYPT_FAIL ,
EMBER_COUNTER_MAC_DROP_IN_MEMORY ,
EMBER_COUNTER_MAC_DROP_IN_FRAME_COUNTER ,
EMBER_COUNTER_MAC_DROP_IN_DECRYPT ,
EMBER_COUNTER_NWK_OUT_FORWARDING ,
EMBER_COUNTER_NWK_IN_SUCCESS ,
EMBER_COUNTER_NWK_DROP_IN_WRONG_SOURCE ,
EMBER_COUNTER_NWK_DROP_IN_FORWARDING ,
EMBER_COUNTER_UART_IN_DATA ,
EMBER_COUNTER_UART_IN_MANAGEMENT ,
EMBER_COUNTER_UART_IN_FAIL ,
EMBER_COUNTER_UART_OUT_DATA ,
EMBER_COUNTER_UART_OUT_MANAGEMENT ,
EMBER_COUNTER_UART_OUT_FAIL ,
EMBER_COUNTER_ROUTE_2_HOP_LOOP ,
EMBER_COUNTER_BUFFER_ALLOCATION_FAIL ,
EMBER_ASH_V3_ACK_SENT ,
EMBER_ASH_V3_ACK_RECEIVED ,
EMBER_ASH_V3_NACK_SENT ,
EMBER_ASH_V3_NACK_RECEIVED ,
EMBER_ASH_V3_RESEND ,
EMBER_ASH_V3_BYTES_SENT ,
EMBER_ASH_V3_TOTAL_BYTES_RECEIVED ,
EMBER_ASH_V3_VALID_BYTES_RECEIVED ,
EMBER_ASH_V3_PAYLOAD_BYTES_SENT ,
EMBER_COUNTER_TYPE_COUNT
}
Define the event counters that can be requested from the application using emberGetCounter() More...
enum EmberPhyType {
EMBER_RADIO_CONFIGURATOR ,
EMBER_STANDARD_PHY_2_4GHZ ,
EMBER_STANDARD_PHY_915MHZ ,
EMBER_STANDARD_PHY_863MHZ
}
Define the PHY configuration of connect stack. More...
enum EmberCalType {
EMBER_CAL_TEMP_VCO = 0x00000001,
EMBER_CAL_IRCAL = 0x00010000,
EMBER_CAL_ALL = 0x00010001
}
Define the type of calibration requested. More...
enum EmberTxStreamParameters {
TX_STREAM_PN9 ,
TX_STREAM_CW
}
Radio Stream mode. More...

Functions

uint8_t * emberKeyContents ( EmberKeyData *key)
This macro allows the programmer to gain access to the key data bytes of the EmberKeyData structure. More...

Detailed Description

Definitions of Connect data types used by various Connect API functions.

See ember-types.h for source code.

Macro Definition Documentation

◆ EMBER_BROADCAST_ADDRESS

#define EMBER_BROADCAST_ADDRESS 0xFFFF

Broadcast address.

Definition at line 75 of file ember-types.h .

◆ EMBER_CAL_INVALID_VALUE

#define EMBER_CAL_INVALID_VALUE (0xFFFFFFFF)

Definition at line 787 of file ember-types.h .

◆ EMBER_COORDINATOR_ADDRESS

#define EMBER_COORDINATOR_ADDRESS 0x0000

The coordinator short address.

Definition at line 82 of file ember-types.h .

◆ EMBER_ENCRYPTION_KEY_SIZE

#define EMBER_ENCRYPTION_KEY_SIZE 16

Size of an encryption key in bytes (16).

Definition at line 51 of file ember-types.h .

◆ EMBER_NULL_NODE_ID

#define EMBER_NULL_NODE_ID 0xFFFF

A distinguished network ID that will never be assigned to any node. Used to indicate the absence of a node ID.

Definition at line 72 of file ember-types.h .

◆ EMBER_USE_LONG_ADDRESS

#define EMBER_USE_LONG_ADDRESS 0xFFFE

Special short address indicating the node should use long addressing as source address.

Definition at line 79 of file ember-types.h .

◆ EUI64_SIZE

#define EUI64_SIZE 8

Size of EUI64 (an IEEE address) in bytes (8).

Definition at line 46 of file ember-types.h .

◆ EXTENDED_PAN_ID_SIZE

#define EXTENDED_PAN_ID_SIZE 8

Size of an extended PAN identifier in bytes (8).

Definition at line 41 of file ember-types.h .

Typedef Documentation

◆ EmberBuffer

typedef uint16_t EmberBuffer

Buffers used by the memory buffer system.

Definition at line 742 of file ember-types.h .

◆ EmberEUI64

typedef uint8_t EmberEUI64[ EUI64_SIZE ]

EUI 64-bit ID (IEEE 802.15.4 long address).

Definition at line 56 of file ember-types.h .

◆ EmberEventData

◆ EmberMessageLength

typedef uint8_t EmberMessageLength

Message length in bytes.

Definition at line 202 of file ember-types.h .

◆ EmberNodeId

typedef uint16_t EmberNodeId

IEEE 802.15.4 node ID. Also known as short address.

Definition at line 61 of file ember-types.h .

◆ EmberPanId

typedef uint16_t EmberPanId

IEEE 802.15.4 PAN ID.

Definition at line 66 of file ember-types.h .

◆ EmberTaskId

typedef uint8_t EmberTaskId

An identifier for a task.

Definition at line 523 of file ember-types.h .

◆ Event

typedef struct Event_s Event

◆ EventQueue

An event queue is currently just a list of events ordered by execution time.

Enumeration Type Documentation

◆ anonymous enum

anonymous enum

Define tasks that prevent the stack from sleeping.

Enumerator
EMBER_OUTGOING_MESSAGES

Messages are waiting for transmission.

EMBER_INCOMING_MESSAGES

One or more incoming messages are processed.

EMBER_RADIO_IS_ON

The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices, i.e., EMBER_STAR_COORDINATOR , EMBER_STAR_RANGE_EXTENDER , EMBER_STAR_END_DEVICE , or EMBER_MAC_MODE_DEVICE , the radio is always on.

EMBER_ASSOCIATING

The node is currently trying to associate to a Connect network.

EMBER_SCANNING

The node is currently performing a MAC-level scanning procedure.

Definition at line 606 of file ember-types.h .

◆ EmberCalType

Define the type of calibration requested.

Enumerator
EMBER_CAL_TEMP_VCO

Temperature calibration

EMBER_CAL_IRCAL

Image Rejection calibration

EMBER_CAL_ALL

Both calibrations

Definition at line 771 of file ember-types.h .

◆ EmberChildFlags

Child flags.

Enumerator
EMBER_CHILD_FLAGS_DEVICE_IS_RANGE_EXTENDER_BIT

The child is a range extender.

EMBER_CHILD_FLAGS_DEVICE_IS_SLEEPY_BIT

The child is a sleepy end device.

EMBER_CHILD_FLAGS_HAVE_PENDING_DATA_BIT

The node has data pending for the child.

EMBER_CHILD_FLAGS_AES_SECURITY_CAPABLE_BIT

The child supports AES-based security.

EMBER_CHILD_FLAG_DEVICE_IS_EXTENDED_BIT

The child is connected through range extender.

Definition at line 181 of file ember-types.h .

◆ EmberCounterType

Define the event counters that can be requested from the application using emberGetCounter()

Enumerator
EMBER_COUNTER_PHY_IN_PACKETS

Every packet that comes in over the radio (except MAC ACKs).

EMBER_COUNTER_PHY_OUT_PACKETS

Every packet that goes out over the radio (except MAC ACKs).

EMBER_COUNTER_MAC_IN_UNICAST

Incoming MAC layer unicasts.

EMBER_COUNTER_MAC_IN_BROADCAST

Incoming MAC layer broadcasts.

EMBER_COUNTER_MAC_OUT_UNICAST_NO_ACK

Outgoing MAC layer unicasts that do not require an ACK.

EMBER_COUNTER_MAC_OUT_UNICAST_ACK_SUCCESS

Outgoing MAC layer unicasts that required an ACK, for which an ACK was received (possibly after retrying).

EMBER_COUNTER_MAC_OUT_UNICAST_ACK_FAIL

Outgoing MAC layer unicasts that required an ACK, for which an ACK was never received (even after retrying).

EMBER_COUNTER_MAC_OUT_UNICAST_CCA_FAIL

Outgoing MAC layer packets which were never transmitted because clear channel assessment always returned busy.

EMBER_COUNTER_MAC_OUT_UNICAST_RETRY

Outgoing MAC layer unicast retries. This does not count the initial transmission. Note a single MAC transmission can result in multiple retries.

EMBER_COUNTER_MAC_OUT_BROADCAST

Outgoing MAC layer broadcasts

EMBER_COUNTER_MAC_OUT_BROADCAST_CCA_FAIL

Outgoing MAC layer broadcasts which were never transmitted because clear channel assessment always returned busy.

EMBER_COUNTER_MAC_OUT_ENCRYPT_FAIL

Outgoing MAC layer messages which were not transmitted due to security error e.g. because security key was not set.

EMBER_COUNTER_MAC_DROP_IN_MEMORY

Dropped incoming MAC layer packets (out of memory)

EMBER_COUNTER_MAC_DROP_IN_FRAME_COUNTER

Dropped incoming MAC layer packets (invalid frame counter)

EMBER_COUNTER_MAC_DROP_IN_DECRYPT

Dropped incoming MAC layer packets (can't decrypt)

EMBER_COUNTER_NWK_OUT_FORWARDING

Outgoing Network layer forwarded packets

EMBER_COUNTER_NWK_IN_SUCCESS

Incoming Network layer data frames correctly processed

EMBER_COUNTER_NWK_DROP_IN_WRONG_SOURCE

Dropped incoming Network layer packets (wrong source node)

EMBER_COUNTER_NWK_DROP_IN_FORWARDING

Dropped incoming Network layer packets (can't forward)

EMBER_COUNTER_UART_IN_DATA

NCP UART in data packet

EMBER_COUNTER_UART_IN_MANAGEMENT

NCP UART in management packet

EMBER_COUNTER_UART_IN_FAIL

NCP UART in frame errors

EMBER_COUNTER_UART_OUT_DATA

NCP UART out data packet

EMBER_COUNTER_UART_OUT_MANAGEMENT

NCP UART out management packet

EMBER_COUNTER_UART_OUT_FAIL

NCP UART out frame errors

EMBER_COUNTER_ROUTE_2_HOP_LOOP
EMBER_COUNTER_BUFFER_ALLOCATION_FAIL
EMBER_ASH_V3_ACK_SENT

ASHv3 ACK frame sent

EMBER_ASH_V3_ACK_RECEIVED

ASHv3 ACK frame received

EMBER_ASH_V3_NACK_SENT

ASHv3 NACK frame sent

EMBER_ASH_V3_NACK_RECEIVED

ASHv3 NACK frame received

EMBER_ASH_V3_RESEND

ASHv3 resends of frames that were not acked

EMBER_ASH_V3_BYTES_SENT

ASHv3 number of bytes sent

EMBER_ASH_V3_TOTAL_BYTES_RECEIVED

ASHv3 number of bytes received

EMBER_ASH_V3_VALID_BYTES_RECEIVED

ASHv3 number of valid bytes received

EMBER_ASH_V3_PAYLOAD_BYTES_SENT

ASHv3 number of payload bytes sent

EMBER_COUNTER_TYPE_COUNT

A placeholder giving the number of Ember counter types.

Definition at line 629 of file ember-types.h .

◆ EmberEventUnits

Either marks an event as inactive or specifies the units for the event execution time.

Enumerator
EMBER_EVENT_INACTIVE

The event is not scheduled to run.

EMBER_EVENT_MS_TIME

The execution time is in approximate milliseconds.

EMBER_EVENT_QS_TIME

The execution time is in 'binary' quarter seconds (256 timer ticks).

EMBER_EVENT_MINUTE_TIME

The execution time is in 'binary' minutes (65536 timer ticks).

EMBER_EVENT_ZERO_DELAY

The event is scheduled to run at the earliest opportunity.

Definition at line 504 of file ember-types.h .

◆ EmberMacAddressMode

802.15.4 addressing mode.

Enumerator
EMBER_MAC_ADDRESS_MODE_NONE

No address on this field.

EMBER_MAC_ADDRESS_MODE_SHORT

Short addressing mode.

EMBER_MAC_ADDRESS_MODE_LONG

Long addressing mode.

Definition at line 321 of file ember-types.h .

◆ EmberMessageOptions

Message options.

Enumerator
EMBER_OPTIONS_NONE

No options.

EMBER_OPTIONS_SECURITY_ENABLED

The packet should be sent out encrypted.

EMBER_OPTIONS_ACK_REQUESTED

An acknowledgment should be requested for the outgoing packet.

EMBER_OPTIONS_HIGH_PRIORITY

The packet should be sent with high priority. High priority messages are added to the head of transmit queue, other messages are added to the tail.

EMBER_OPTIONS_INDIRECT

The packet should be sent via the indirect queue. This option only applies to nodes with EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE node type.

Definition at line 208 of file ember-types.h .

◆ EmberNetworkStatus

Defines the possible join states for a node.

Enumerator
EMBER_NO_NETWORK

The node is not associated with a network in any way.

EMBER_JOINING_NETWORK

The node is currently attempting to join a network.

EMBER_JOINED_NETWORK

The node is joined to a network.

EMBER_RADIO_TEST

The node is currently using its radio for test

Definition at line 145 of file ember-types.h .

◆ EmberNodeType

Define the possible types of nodes and the roles that a node might play in a network.

Enumerator
EMBER_UNKNOWN_DEVICE

Device is not in network.

EMBER_STAR_COORDINATOR

Extended star mode device: Will relay messages and can act as a parent to range extender and end device nodes. A node can be started as a coordinator using the emberFormNetwork() API.

EMBER_STAR_RANGE_EXTENDER

Extended star mode device: Will relay messages and can act as a parent to end device nodes. Joins to a coordinator. A node can be started as a range extender using the emberJoinNetwork() or emberJoinNetworkExtended() API.

EMBER_STAR_END_DEVICE

Extended star mode device: Communicates only with its parent and will not relay messages. A node can be started as an end device using the emberJoinNetwork() or emberJoinNetworkExtended() API.

EMBER_STAR_SLEEPY_END_DEVICE

Extended star mode device: An end device whose radio is turned off when not communicating to save power. The application must call emberPollForData() to receive messages. A node can be started as a sleepy end device using the emberJoinNetwork() or emberJoinNetworkExtended() API.

EMBER_DIRECT_DEVICE

Direct mode device: A device able to send and receive messages from other devices in range on the same PAN ID, with no star topology restrictions. Such device does not relay messages. A node can be started as a direct device by using the emberJoinCommissioned() API.

EMBER_MAC_MODE_DEVICE

MAC mode device: A device able to send and receive MAC-level messages. A node can be started as a MAC mode device by using the emberJoinCommissioned() , the emberJoinNetworkExtended() or the emberMacFormNetwork() API.

EMBER_MAC_MODE_SLEEPY_DEVICE

MAC mode device: A sleepy device able to send and receive MAC-level messages. The radio on the device is turned off when not communicating. The application must call emberPollForData() to receive messages. A node can be started as a sleepy MAC mode device by using the emberJoinCommissioned() API or the emberJoinNetworkExtended() API.

Definition at line 89 of file ember-types.h .

◆ EmberPhyType

Define the PHY configuration of connect stack.

Enumerator
EMBER_RADIO_CONFIGURATOR

Connect uses radio configurator PHY

EMBER_STANDARD_PHY_2_4GHZ

Connect is configured to use only 2.4GHz standard PHY

EMBER_STANDARD_PHY_915MHZ

Connect is configured to use only 915MHz standard PHY

EMBER_STANDARD_PHY_863MHZ

Connect is configured to use only 863MHz standard PHY

Definition at line 748 of file ember-types.h .

◆ EmberTxStreamParameters

Radio Stream mode.

Enumerator
TX_STREAM_PN9

Pseudo random PN9 byte sequence

TX_STREAM_CW

An unmodulated carrier wave

Definition at line 857 of file ember-types.h .

Function Documentation

◆ emberKeyContents()

uint8_t* emberKeyContents ( EmberKeyData * key )

This macro allows the programmer to gain access to the key data bytes of the EmberKeyData structure.

Parameters
[in] key A Pointer to an EmberKeyData structure.
Returns
uint8_t* Returns a pointer to the first byte of the key data.