A structure that describes the addressing fields of a 802.15.4 frame. More...

#include < ember-types.h >

Data Fields

EmberMacAddress srcAddress
EmberMacAddress dstAddress
EmberPanId srcPanId
EmberPanId dstPanId
bool srcPanIdSpecified
bool dstPanIdSpecified

A structure that describes the addressing fields of a 802.15.4 frame.

Definition at line 359 of file ember-types.h .

Field Documentation

◆ dstAddress

EmberMacAddress EmberMacFrame::dstAddress

An EmberMacAddress structure indicating the destination address of a MAC frame.

Definition at line 368 of file ember-types.h .

◆ dstPanId

EmberPanId EmberMacFrame::dstPanId

An EmberPanId struct indicating the destination PAN ID of a MAC frame. This field is meaningful only if dstPanIdSpecified is set to true.

Definition at line 378 of file ember-types.h .

◆ dstPanIdSpecified

bool EmberMacFrame::dstPanIdSpecified

True if the dstPanId field is set, false otherwise.

Definition at line 386 of file ember-types.h .

◆ srcAddress

EmberMacAddress EmberMacFrame::srcAddress

An EmberMacAddress structure indicating the source address of a MAC frame.

Definition at line 363 of file ember-types.h .

◆ srcPanId

EmberPanId EmberMacFrame::srcPanId

An EmberPanId struct indicating the source PAN ID of a MAC frame. This field is meaningful only if srcPanIdSpecified is set to true.

Definition at line 373 of file ember-types.h .

◆ srcPanIdSpecified

bool EmberMacFrame::srcPanIdSpecified

True if the srcPanId field is set, false otherwise.

Definition at line 382 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h