The static part of an event. Each event can be used with only one event queue. More...

#include < ember-types.h >

Data Fields

struct EventQueue_s * queue
void(* handler )(struct Event_s *)
void(* marker )(struct Event_s *)
const char * name

The static part of an event. Each event can be used with only one event queue.

Definition at line 536 of file ember-types.h .

Field Documentation

◆ handler

void(* EventActions::handler) (struct Event_s *)

Definition at line 538 of file ember-types.h .

◆ marker

void(* EventActions::marker) (struct Event_s *)

Definition at line 539 of file ember-types.h .

◆ name

const char* EventActions::name

Definition at line 540 of file ember-types.h .

◆ queue

struct EventQueue_s * EventActions::queue

Definition at line 537 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h